MPC5634M-OPWFM-SAIC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5634M-OPWFM-SAIC

840 Views
陈秀侠
Contributor II

Now  I  wanted to generate EMIOS OPWFM,and using EMIOS SAIC  module for capturing   frequency. On demo boads I connect pads between them.

But I can't generate OPWFM, I don't why?

Here my code:

///////////////////////////////////////////////////////////////////////////////////

/**********************************************************************

Function  :eMIOS_Init初始化函数

Parameters:*ConfigPtr

return    :None.

**********************************************************************/

void eMIOS_Init(const eMIOS_ConfigType* ConfigPtr)

{

  eMIOS_ChannelType Chn = ConfigPtr->eMIOS_Channel;

 

 

    /* 禁能分频器 */

    //EMIOS.MCR.B.GPREN = 0;

 

 

  if(PWM_MODE == ConfigPtr->eMIOS_Mode)

  {

  /* 设置管脚通道为PWM功能 */

  SIU.PCR[Chn + 179].B.PA  = 1;

  SIU.PCR[Chn + 179].B.OBE = 1;

 

     /* 禁能分频器 */

     EMIOS.MCR.B.GPREN = 0;

 

 

  /* eMIOS模块进入正常工作模式 */

     EMIOS.MCR.B.MDIS = 0;

    

     /* eMIOS模块全局64分频 */

     EMIOS.MCR.B.GPRE = 63;

    

     /* 禁止外部时基,设置通道23作为总线A控制时基 */

     EMIOS.MCR.B.ETB = 0;

    

     /* 使能全局时基 */

     EMIOS.MCR.B.GTBE = 1;

    

     EMIOS.MCR.B.FRZ = 1;

    

     /* 使能全局分频器 */

     //EMIOS.MCR.B.GPREN= 1;

 

     /* eMIOS模式为:OPWFM */

     EMIOS.CH[Chn].CCR.B.MODE = 0x19;

     //EMIOS.CH[Chn].CCR.B.MODE = 0x60;

    

    

  /* 使用内部时钟计数器 */

     EMIOS.CH[Chn].CCR.B.BSL  = 0;

    

     /* 使能内部时钟分频 */

     EMIOS.CH[Chn].CCR.B.UCPREN = 1;

    

     /* 设置通道内部时钟分频值为1 */

     EMIOS.CH[Chn].CCR.B.UCPRE = 0;

 

 

  /* 设置极性:匹配A时输出0,匹配B时输出1 */

     EMIOS.CH[Chn].CCR.B.EDPOL = 0;

 

 

     /* 使能全局分频器 */

     EMIOS.MCR.B.GPREN= 1;

  }

  else

  {

  /* 设置管脚通道为PWM功能 */

  SIU.PCR[Chn + 179].B.PA  = 1;

  SIU.PCR[Chn + 179].B.IBE = 1;

#if 1

     /* 禁能分频器 */

     //EMIOS.MCR.B.GPREN = 0;

    

     /* eMIOS模块进入正常工作模式 */

  EMIOS.MCR.B.MDIS = 0;

 

     /* eMIOS模块全局64分频 */

  EMIOS.MCR.B.GPRE = 63;

 

  /* 禁止外部时基,设置通道23作为总线A控制时基 */

  EMIOS.MCR.B.ETB = 0;

 

 

     /* 使能全局时基 */

  EMIOS.MCR.B.GTBE = 1;

 

     /* 使能全局分频器 */

  EMIOS.MCR.B.GPREN = 1;

#endif

  /* 设置为ICU模式 */

  EMIOS.CH[Chn].CCR.B.MODE = 0x02;

 

  /* 使用内部时钟计数器 */

  EMIOS.CH[Chn].CCR.B.BSL = 0x3;

 

 

     /* 使能内部时钟分频 */

  EMIOS.CH[Chn].CCR.B.UCPREN = 1;

 

  /* 使能中断 */

  EMIOS.CH[Chn].CCR.B.FEN = 1;

 

     /* 设置通道内部时钟分频值为1 */

  EMIOS.CH[Chn].CCR.B.UCPRE = 0;

 

 

  /* 上升沿触发 */

  EMIOS.CH[Chn].CCR.B.EDSEL = 0x0;

  EMIOS.CH[Chn].CCR.B.EDPOL = 0x1;

 

     /* 使能全局分频器 */

  //EMIOS.MCR.B.GPREN = 1;

  }

 

  //EMIOS.MCR.B.GPREN = 1;

}

 

 

 

 

/*******************************************************************

* FUNCTION :    Pwm_Output                                        *

*                                                                 *

* DESCRIPTION : Set channel, Period and DutyCycle, for example,   *

*               your choice is channel 0, period=2s,              *

*               dutycycle=50%, you should input                   *

*               (0,2000000,1000000),0.5=1,000,000/2,000,000       *

*               Note :the clk is 1MHz, 1000 clocks =1 ms          *

*                                                                 *

* INPUTS :      -Chn: Range from 0 to 22                          *

*               -Period: Type uint32                              *

*               -DutyCycle: Type uint32                           *

*******************************************************************/

void eMIOS_SetPeriodAndDuty(eMIOS_ChannelType Chn, eMIOS_PeriodType Period, uint32 DutyCycle)

{

  if(Period == 0)

  {

  EMIOS.CH[Chn].CBDR.R = 0;

  EMIOS.CH[Chn].CADR.R = 0;

  }

  else

  {

  if(DutyCycle == 0)

  {

  EMIOS.CH[Chn].CBDR.R = Period;

  EMIOS.CH[Chn].CADR.R = 0;

  }

  else if(DutyCycle >= Period)

  {

  EMIOS.CH[Chn].CBDR.R = Period;

  EMIOS.CH[Chn].CADR.R = Period;

  }

  else

  {

  EMIOS.CH[Chn].CBDR.R = Period;

  EMIOS.CH[Chn].CADR.R = Period - DutyCycle;

  }

  }

}

 

 

 

 

uint32 eMIOS_GetIcuFrequency(eMIOS_ChannelType Chn)

{

  uint32 IcuFrequency = 0;

  uint32 IcuFrequencyCount = 0;

 

  if(eMIOSIcuPeriod[Chn].IcuPeriodSecond >= eMIOSIcuPeriod[Chn].IcuPeriodFirst)

  {

  IcuFrequencyCount = eMIOSIcuPeriod[Chn].IcuPeriodSecond - eMIOSIcuPeriod[Chn].IcuPeriodFirst;

  }

  else

  {

  IcuFrequencyCount = (0x00FFFFFF - eMIOSIcuPeriod[Chn].IcuPeriodFirst) + eMIOSIcuPeriod[Chn].IcuPeriodSecond;

  }

 

  if(0 == IcuFrequencyCount)

  {

  IcuFrequency = 0;

  }

  else

  {

  /* eMIOS内部频率为1MHz */

  IcuFrequency = (uint32)(1000000/IcuFrequencyCount);

  }

 

 

  return IcuFrequency;

}

 

 

 

 

void eMIOS_ReadIcuPeriod(eMIOS_ChannelType Chn)

{

  while(EMIOS.CH[Chn].CSR.B.FLAG == 0)

  {

  ;

  }

  eMIOSIcuPeriod[Chn].IcuPeriodFirst  = eMIOSIcuPeriod[Chn].IcuPeriodSecond;

  eMIOSIcuPeriod[Chn].IcuPeriodSecond = EMIOS.CH[Chn].CADR.R;

}

 

 

 

 

void eMIOS_IcuIrq0(void)

{

  eMIOS_ReadIcuPeriod(eMIOS_0);

  EMIOS.CH[eMIOS_0].CSR.B.FLAG = 1;

}

 

 

 

 

void eMIOS_IcuIrq2(void)

{

  eMIOS_ReadIcuPeriod(eMIOS_2);

  EMIOS.CH[eMIOS_2].CSR.B.FLAG = 1;

}

///////////////////////////////////////////////////////////////////

Is there any example for MPC5634-OPWFM-SAIC?

Thank you!

Original Attachment has been moved to: MPC5634-OPWFM-SAIC.rar

Labels (1)
0 Kudos
1 Reply

381 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

See https://community.freescale.com/thread/383966 that probably helps you.

BR, Petr

0 Kudos