Using T1024RDB, how To enable Atheros wireless driver (802.11ac) for linux 3.12.19-rt30

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using T1024RDB, how To enable Atheros wireless driver (802.11ac) for linux 3.12.19-rt30

1,170 Views
sri-cdot
Contributor I

Hi, I am using T1024RDB, I am trying to enable Atheros wireless driver (802.11ac), for linux  3.12.19-rt30 then we are facing issue. The linux is not coming up, showing the below error. It says, unable to fetch board data, firmware files. Please help to rectify this error.

ath10k_pci 0000:01:00.0: BAR 0: assigned [mem 0xc00000000-0xc001fffff 64bit]

ath10k: MSI-X didn't succeed (1), trying MSI

ath10k: MSI interrupt handling

ath10k: Hardware name qca988x hw2.0 version 0x4100016c

ath10k: could not fetch board data (-2)

ath10k: could not fetch firmware files (-2)

ath10k: could not probe fw (-2)

ath10k: could not register driver core (-2)

ath10k: early firmware event indicated

Unable to handle kernel paging request for data at address 0x00000010

Faulting instruction address: 0xc00000000057b5cc

Regards,

Sridhar

Labels (1)
0 Kudos
1 Reply

760 Views
bpe
NXP Employee
NXP Employee

See this community post:

t1023 freescale board (using SDK 1.9). With default image, wireless chipset (AR9558) was not detect...


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos