Hi,
Working with FreeMASTER WCT GUI Auto A13 .Having difficulty finding RunTimeparams descriptions in online or in Freescale Documentations. Would greatly appreciate Help .
Thanks
Santosh
Solved! Go to Solution.
Hi Santosh,
See below:
Input power: RunTimeParams[0].dwCalculatedInputPower.
Input power = rail voltage * input current.
Customer also can get rail voltage and input current in application and then multiply them.
Call WCT_AnalogIoGetInputCurrent() to get input current and WCT_AnalogIoGetRailVoltage() to get rail voltage.
TX estimated internal power loss: RunTimeParams[0].swTxInternalLoss
Consumed Power for RX: RunTimeParams[0].dwRxReportedPower
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Can you have a look to:
http://cache.freescale.com/files/microcontrollers/doc/user_guide/WCT100XARTDUG_V3.3.pdf
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
Thank You very much , Appreciate your kind Help.
The Document you have sujjested provides good information about Caliberating, Debugging of Fressscale MASTER GUI for AUTO A13 and NvmParams
descreption.
It would be great if you can sujjest a document where one can find the RunTimeParms descreptions just like
NvmParams descreption which are available in the document you sujjested.
for example:
the System parameter "Keyfob Avoidance Duration (ms)"
is neatly detailed as below in document
Details:
This parameter defines the length of time the unit will operate at the Keyfob Avoidance Frequency after being
triggered by the IO control signal. This value is ignored if the Keyfob Avoidance Duration Based on IO parameter is
TRUE.
Default Value:
100
Min Value:
0
Max Value:
65535
Member:
NvmParams.SystemParams.OpStateParams.wKeyfobAvoidanceDurationMs
Similarly if one wants to know what does RunTimeparams[0].bySignalStrength or any other RunTimeparams[0].xxxxxxx mean .where can one look for the parameter description?
Thanks & Best Regards,
Santosh
Hi Santosh,
I've installed the WCT100xA_A13_V3.4
The RUNTIME_PARAMS stucture is defined in the wct_LibStruct.h.
I don't find information related to the RUNTIME_PARAMS stucture.
Don't know if this will help you but there are some entries for RUNTIMEPARAMS in the devnotes.txt
I will check with colleague to see if I can get more info.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
Many many Thanks for your Inputs and happy that you understood the needs.
I am Greatfull to you and your collages at Freescale
Looked into the RUNTIME_PARAMS structure defined in the wct_LibStruct.h and the entries for RUNTIMEPARAMS in devnotes.txt these were of little help .
Any further Information regarding the RUNTIME_PARAMS definitions will be very helpfull and greatly appreciated.
Thanks & Best Regards,
Santosh
Hi Santhosh,
I got feedback from the Technical writer:
Variables in RUNTIME_PARAMS are used in internal library, and customer don’t need to care about it.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
Thank You once again.
The purpose of my query was to find out the definitions of Variables being used in Freemaster GUI at Run Time which appear at bottom right corner of the GUI and understand what values are being dumped into these variables from the board.
Except the NvmParams.[ 0].xxxxxxxxx definitions in Debug user guide one cannot find other variable definitions which are used by WCTAutoA13_WCT1003A.pmp GUI .I have to understand them for my application development .
Kindly provide your valuable help.
Thanks & Best Regards,
Santosh
Hi Santhosh,
Sorry for the delay ... just got feedback:
Runtime variables in FreeMASTER are used for our debugging.
If customer wants to use them for their application, please describe their application requirement,
then I will suggest them to use which variable and give the definitions.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
Thank You once again for your Reply.
For our application we are required to measure the Input Power , Output Power ,Power Loss and Consumed Power for Mobile Phone charging .
Can you sujjest wich Run Time parameters or Normal Parameters can be used to obtain the above data.
or kindly provide the definitions of Run Time parameters to obtain above mentioned parameters.
Thanks & Best Regards,
Santosh
Hi Santosh,
See below:
Input power: RunTimeParams[0].dwCalculatedInputPower.
Input power = rail voltage * input current.
Customer also can get rail voltage and input current in application and then multiply them.
Call WCT_AnalogIoGetInputCurrent() to get input current and WCT_AnalogIoGetRailVoltage() to get rail voltage.
TX estimated internal power loss: RunTimeParams[0].swTxInternalLoss
Consumed Power for RX: RunTimeParams[0].dwRxReportedPower
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
Thank You very much for your support .I was exactly searching all the while for the above parameter definitions.
In Freemaster GUI it was difficult with so many RUN Time Parameters to figure out the correct one .
Your answer has helped a lot in going further with our application.
Thanks & Best Regards,
Santosh
You're welcome.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
New Year Greetings!
Looking for help in regard to Input Current Calibration of WCT 5WTXAUTO in FreeMaster .
Following the instructions from
WCT 1001A/WCT1003A Run -Time Debugging User’s Guide ,Tried to do the Input Curent Calibration of WCT 5WTXAUTO But the board after entering into debug mode does not allow for the receiver to get power.i.e no power at receiver.
So unable to change diffferent load currents as per the sujjestion in the above document.
can you sujjest a way.
Best Regards,
Santosh Reddy Pulasani
Hi,
Thanks.
wish you an happy new year too.
this will be handled through Error in Input Curent Calibration of WCT 5WTXAUTO
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal ,
Thank You .I was not 100% sure if CodeWarrior for MCU Team were
responsible for FreeMASTER so I mailed you also.
Best Regards,
Santosh Reddy Pulasani
Am 11.01.2016 um 15:53 schrieb trytohelp:
>
NXP Community
<http://jiveon.jivesoftware.com/mpss/c/5gA/PDcDAA/t.1tq/W2OGCMceRAqASSXEmmKPmQ/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQJ6kyiZ2Cef2qt-2B2uYN1YnWHaJNGi7m0dsLcrT7D0aEsRC9ydi8bGmPSoTrNqropzOzEJWlRcWGPjR3DG2V-2Fd9JgazgrYhAttaPsLKIUR-2FzQ-3D-3D>
>
Where to find RunTime Parameters definitions of FreeMASTER WCT GUI
for Auto A13
reply from Pascal Irrle
<http://jiveon.jivesoftware.com/mpss/c/5gA/PDcDAA/t.1tq/W2OGCMceRAqASSXEmmKPmQ/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRgmK5SVFHx0RkfidtBoWqLxOii3XKwzh7tVeWRC-2BTmBK0bJLMgQQbVDaPRAU5Qf70-3D>
in /CodeWarrior for MCU/ - View the full discussion
<http://jiveon.jivesoftware.com/mpss/c/5gA/PDcDAA/t.1tq/W2OGCMceRAqASSXEmmKPmQ/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bR3nTg9CBZ-2BaC-2BW0rdwOkE-2FduiLVeMOZtD1AJ3-2FAd02MsWZzfSs7q-2B9lUnp5dyfnOU-3D>
>