Reg usb cam error in imx6q sabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reg usb cam error in imx6q sabresd

1,217 Views
shalinikp
Contributor II

Logitech USB webcam connected to imx6q board is getting connected. But if I launch any of the application to test webcam, the port resets and the webcam is getting disconnected.  Please help me on this. Below is the error I'm getting

#fswebcam

ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  hub 1-0:1.0: Cannot enable port 1.  Maybe the USB cable is bad?
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110
  ci_hdrc ci_hdrc.0: port 1 reset error -110

But the same webcam is working fine in PC. ANd also when I connect USB keyboard/mouse to board there is no error.

Labels (3)
0 Kudos
3 Replies

565 Views
igorpadykov
NXP Employee
NXP Employee

Hi shalini

first try to verify if this camera is uvc camera.

Also it may be necessary to modprobe driver for camera before usage:

Using a USB Camera with GStreamer

Re: mx6q usb camera

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

565 Views
shalinikp
Contributor II

Hi,

   Thanks for d reply.  It is a UVC camera. Camera driver is added. can see "dev/video0". The problem is the port is getting reset and webcam is getting disconnected.

0 Kudos

565 Views
igorpadykov
NXP Employee
NXP Employee

one can try with Demo image :

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

0 Kudos