Does i.MX6DL's HDMI support 4k x 2k resolution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6DL's HDMI support 4k x 2k resolution?

Jump to solution
1,797 Views
chaohuang
Contributor I

Hi, Everybody

     I see the spec that iMX6's hdmi support 4k x 2k video format. But I can not see it in 33-3 table.

     My question is whether iMX6's hdmi support 3840x2160@30hz resolution(the fps can be less than 30)?

     Thank you in advance for your answer.

Regards,

Chao

Labels (3)
0 Kudos
1 Solution
1,056 Views
igorpadykov
NXP Employee
NXP Employee

HI Chao

unfortunately not as IPU max. supported screen size: up to 4096 x 2048 pixels,

HDMI is connected to IPU as shown on p.15,17 presentation

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

4 Replies
1,057 Views
igorpadykov
NXP Employee
NXP Employee

HI Chao

unfortunately not as IPU max. supported screen size: up to 4096 x 2048 pixels,

HDMI is connected to IPU as shown on p.15,17 presentation

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,056 Views
julienc
Contributor II

Hi, 

I tried to create a screen of 4096x2048 with fbset on wandboard with iMx6DualLite : 

 - fbset -g 4096 2048 4096 2160 32 -t 4500 4 4 4 4 12 4

I have some error with DI0 counter because the DIO counter have only 12 bits resolution (DI0 Sync Wave Gen 2 Register 0).

imx-ipuv3 2400000.ipu: DI0 for 1 counters out of range.
imx-ipuv3 2400000.ipu: DI0 for 2 counters out of range.

So how i can create a screen of 4096x2048 resolution.

Thanks

Julien

0 Kudos
1,056 Views
chaohuang
Contributor I

Bnd if I don't use IPU to draw the picture, should it support the 4k x 2k resolution?

Thank you!

0 Kudos
1,056 Views
chaohuang
Contributor I

Thank you for your kindly reply! But I am curious about that why some background of the resolution is green and some about white and blue in p 15 of the Document? I can not see any explain in that document... Do you know what does it mean?

Thank you!

0 Kudos