i.MX287: I can't attach my nor flash mtd part to ubi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX287: I can't attach my nor flash mtd part to ubi

Jump to solution
2,323 Views
hwo
Contributor III

Hi all,

When burn the board using MFGTOOL, fails to attach mtd part. Debug trace is:

mx28_nor_flash spi1.0: mx28_nor_flash (32768 Kbytes)

Creating 2 MTD partitions on "mx28_nor_flash":

0x000000000000-0x000000100000 : "boot"

0x000000100000-0x000002000000 : "kernel"

UBI: attaching mtd1 to ubi0

UBI: physical eraseblock size:   4096 bytes (4 KiB)

UBI: logical eraseblock size:    3968 bytes

UBI: smallest flash I/O unit:    1

UBI: VID header offset:          64 (aligned 64)

UBI: data offset:                128

UBI error: ubi_read_volume_table: the layout volume was not found

UBI error: ubi_init: cannot attach mtd1

I use a Winbond nor flash(W25Q256FVFIG), kernel version is 2.6.35.3

I debug the attaching process, it seems when read flash PEB's VID header, its magic number doesn't equal to predefined macro UBI_VID_HDR_MAGIC. However the flash read operation is successful.

This confuse me a lot. I searched the Google, most says the filesystem should be ubinized with mtd-utils. But my situation is Kernel just initializes the ubi module, it hasn't come to the mounting of filesystem I think.

Has read the http://www.linux-mtd.infradead.org/faq/ubi.html#L_format_mtd, the website says I needn't to format nor flash before the attaching operation.

I really don't know what happened. Someone familiar with ubi or has came across similar problem?  Possible reason is also appreciated.

Thanks in advance.

#################################################################################################################

Part of the ucl.xml content is:

<LIST name="Singlechip NAND" desc="Install on singlechip NAND">

<CMD type="boot" body="Recovery" file="updater.sb" timeout="60" if="HabDisable">Booting update firmware.</CMD>

<CMD type="boot" body="Recovery" file="updater_ivt.sb" timeout="60" if="HabEnable">Booting update firmware.</CMD>

<CMD type="push" body="mknod class/mtd,mtd0,/dev/mtd0"/>                            ----------------------tool's log stops here with hint(

Panel A Start <CMD/> type="push" body="mknod class/mtd,mtd0,/dev/mtd0" file="" timeout="10" onError="" text="".

Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE)

<CMD type="push" body="mknod class/mtd,mtd1,/dev/mtd1"/>

<CMD type="push" body="mknod class/misc,ubi_ctrl,/dev/ubi_ctrl"/>

<CMD type="push" body="$ flash_eraseall /dev/mtd0">Erasing rootfs partition</CMD>

<CMD type="push" body="$ flash_eraseall /dev/mtd1">Erasing rootfs partition</CMD>

<CMD type="push" body="send" file="files/imx28_ivt_linux.sb">Sending firmware</CMD>

<CMD type="push" body="$ kobs-ng init $FILE">Flashing firmware</CMD>

<CMD type="push" body="$ ubiattach /dev/ubi_ctrl -m 1 -d 0">Attaching UBI partition</CMD>

<CMD type="push" body="mknod class/ubi,ubi0,/dev/ubi0"/>

<CMD type="push" body="$ ubimkvol /dev/ubi0 -n 0 -N rootfs0 -s 224MiB">Creating UBI volumes</CMD>

<CMD type="push" body="$ ubimkvol /dev/ubi0 -n 1 -N data -m">Creating UBI volumes</CMD>

<CMD type="push" body="$ mkdir -p /mnt/ubi0; mount -t ubifs ubi0_0 /mnt/ubi0" />

<CMD type="push" body="pipe tar -jxv -C /mnt/ubi0" file="files/rootfs.tar.bz2">Transfer rootfs</CMD>

<CMD type="push" body="frf">Finish Flashing NAND</CMD>

<CMD type="push" body="$ umount /mnt/ubi0">Unmounting</CMD>

<CMD type="push" body="$ echo Update Complete!">Done</CMD>

</LIST>

----------------------------------------------kernel cmd below-------------------------------------------------------

Kernel command line: noinitrd console=ttyAM0,115200 ubi.mtd=1 root=ubi0:rootfs0 rootfstype=ubifs rw gpmi

Labels (2)
0 Kudos
1 Solution
989 Views
igorpadykov
NXP Employee
NXP Employee

Hi h

there are issues for using ubifs described below, so one can try to use jffs2

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
990 Views
igorpadykov
NXP Employee
NXP Employee

Hi h

there are issues for using ubifs described below, so one can try to use jffs2

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
989 Views
hwo
Contributor III

Thanks igor!

I'll try jfss2.

One thing I think the nor flash should be formatted before ubi scanning the VID/EC header, otherwise, there's no possibility the magic number equals the predefined macro!  

And hope someday later I can figure out the ubi issue!

0 Kudos