Hi,
I tried to close config my wandboard using Secure boot on Wandboard and I could see at uboot level I have close config
No panel detected: default to HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
=> hab_status
Secure boot enabled
HAB Configuration: 0xcc, HAB State: 0x99
No HAB Events Found!
I dont have my linux kernel enabled with close config certificates like u-boot.
Now when i try to check the snvs register i can see following
SSM_STsnvs-secvio 20cc000.caam-snvs: violation handlers armed - trusted state |
How can set my board to secure state instead of trusted one.
Thanks and Regards,
Swapnil Pendhare.
Solved! Go to Solution.
Hello,
Please check if SEC_CONFIG fuse is burned to close mode.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Please check if SEC_CONFIG fuse is burned to close mode.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------