Hi folks,
I am getting the following issue while running ./ltib on ubuntu12.04
RPM build errors:
Bad exit status from /home/giritharan/extra/ltib/tmp/rpm-tmp.74178 (%build)
Build time for u-boot-v2009.08: 0 seconds
Failed building u-boot-v2009.08
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Thu Oct 22 19:03:41 2015
Ended: Thu Oct 22 19:03:43 2015
Elapsed: 2 seconds
These packages failed to build:
u-boot-v2009.08
Build Failed
Exiting on error or interrupt
thanks in advance..................
Message was edited by: sarathkumar natarajan
Hi sarathkumar
it is necessary to install patches for ubuntu 12.04
Re: What are all the patches need it for LTIB on ubuntu 12.04
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks its woked