I have Freescale Linux SDK v1.8 for QorIQ Processors that I am using to compile source images for p5040ds development system.
I have compiled the u-boot as instructed in below link .
modifying u-boot for QorIQ processors
Now i want to customize Linux Kernel. For this i am using these commands.
bitbake -c cleansstate kernel
I got following output.
Loading cache: 100% |########################################################################################################################################################################| ETA: 00:00:00
Loaded 2366 entries from dependency cache.
ERROR: Nothing PROVIDES 'kernel'. Close matches:
kernelshark
I also run
bitbake kernel -c cleansstate , but got the same output. What is wrong here ?
Solved! Go to Solution.
Use the following command sequence:
$ bitbake -c cleansstate virtual/kernel
$ bitbake -c patch virtual/kernel
Configure kernel.
$ bitbake -c menuconfig virtual/kernel
$ bitbake virtual/kernel // Rebuild kernel:
Note for clean commands:
clean:remove the work folder of the package
•cleansstate:clean+ delete the cached binary
−when a known good package fails to build unexpectedly, or an image build fails with "error: Failed dependencies", do -c cleansstatefirst on the failing package, then rebuild
•patch:install source including all patches
Use with care:
•cleanall: delete the source archive from../sources
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Use the following command sequence:
$ bitbake -c cleansstate virtual/kernel
$ bitbake -c patch virtual/kernel
Configure kernel.
$ bitbake -c menuconfig virtual/kernel
$ bitbake virtual/kernel // Rebuild kernel:
Note for clean commands:
clean:remove the work folder of the package
•cleansstate:clean+ delete the cached binary
−when a known good package fails to build unexpectedly, or an image build fails with "error: Failed dependencies", do -c cleansstatefirst on the failing package, then rebuild
•patch:install source including all patches
Use with care:
•cleanall: delete the source archive from../sources
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------