Run Freescale cloud-connected Zigbee Thermostat Demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run Freescale cloud-connected Zigbee Thermostat Demo

832 Views
dongyangli
Contributor I

We want to run Cloud-Connected zigbee Demo and brought all the tower system boards its suggests:

Freescale Cloud-Connected ZigBee Thermostat Demo

I want to ask about the software we need to compile the software demo. According to demo user guide, are the following softwares needed?

1. IAR Embedded Workbench for ARM v7.10.1 (for K70 and Kw24zigbee)

2. CodeWarrior for MCUs v10.6. (for MC13237zigbee).

MQX RTOS v4.0.2

We program K70 use codewarrior before. Do we need to use IAR to run sw demo? Since we only have Codewarrior now, I wonder is the IAR neccery?

Any suggestions are very grateful. It would br better to list the software enviroment and version. Thank you so much!

0 Kudos
1 Reply

569 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dongyang,

You can use CodeWarrior for MCUs v10.6 to compile the MC13237 project but you will need IAR Embedded Workbench for ARM v7.10.1 for both the K70 and KW24 projects.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos