I'm having a hard time getting an MQX app to run from address 0x15000. I have updated the linker so it builds in that space and set MQX_ROM_VECTROS to false. I should be able to get it to run if I stop at program entry point and do a "move to" at address 0x15000 in Disassembly right? I end up with an unhanded exception.
Hello Michael,
Please check the below thread and let me know if this helps.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
It's getting stuck on the following lines with the K64. Works fine on the K60.
WDOG_UNLOCK = (uint16_t)STARTUP_WDOG_KEY_1; /* Key 1 */
WDOG_UNLOCK = (uint16_t)STARTUP_WDOG_KEY_2; /* Key 2 */