I wonder if there is any wireless or Wifi module compactable with K70_120M. If so is there any demo for it?
Solved! Go to Solution.
Hi,
There are two type KW24 boards: TWR-KW2x and USB-KW24D512.
USB-KW24D512 could work as Zigbee node.
For the Zigbee communication emulation, it need tow boards with KW24 product.
Freescale provides Freescale Kinetis KW2xD IEEE® 802.15.4 Software & Freescale Kinetis KW2xD SMAC Software, which could be downloaded.
Our third partner Silex Technology provides SX-ULPAN-EVK board, which is development board compatible with the Freescale Tower System and is designed to evaluate the Qualcomm Atheros QCA4004 chipset (Ultra-Low-Power Wi-Fi) in conjunction with the Freescale Kinetis MCUs.
More detailed info, please check below link:
Tower System board for QCA4004 based Low Powe|Freescale
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Please refer below document about K70 WiFi application, which is using GT202 WiFi module.
Freescale Cloud-Connected ZigBee Thermostat Demo
The GT202 KIT could be get from below link:
https://parts.arrow.com/es/item/detail/shenzhen-longsys-electronics-co-ltd/gt202kits#EJne
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you so much,
I checked the demo video already, I wonder if I only need Zigbee test,
we should buy a pair of TWR-KW24D512. Is the Qualcomm GT202 combine
with carrier board necessary? Do you have demo only for TWR-KW24D512
communications?
BTW, Do you have more suggestion of wireless modules plugin K70_120M tower?
Thanks again, you are really great help!
Quoting Hui_Ma <admin@e11339.dscb.akamaiedge.net>:
Hui_Ma
replied to the discussion
"wireless or Wifi module compactable with K70_120M tower system?"
To view the discussion, visit:
https://community.freescale.com/message/567643?et=watches.email.thread#567643
>
Hi,
There are two type KW24 boards: TWR-KW2x and USB-KW24D512.
USB-KW24D512 could work as Zigbee node.
For the Zigbee communication emulation, it need tow boards with KW24 product.
Freescale provides Freescale Kinetis KW2xD IEEE® 802.15.4 Software & Freescale Kinetis KW2xD SMAC Software, which could be downloaded.
Our third partner Silex Technology provides SX-ULPAN-EVK board, which is development board compatible with the Freescale Tower System and is designed to evaluate the Qualcomm Atheros QCA4004 chipset (Ultra-Low-Power Wi-Fi) in conjunction with the Freescale Kinetis MCUs.
More detailed info, please check below link:
Tower System board for QCA4004 based Low Powe|Freescale
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------