Porting Ubuntu to IMX6 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting Ubuntu to IMX6 board

1,776 Views
srinivasaraopor
Contributor II

Hi,

We would like to port Ubuntu to IMX6DL board. We are getting the pre-built images only. When we are deploying pre-built images we are not getting all the required files like linux/arch/arm/boot/dts/ doesnot have any dtsi file. some times arch/arm folder itself is not there. it is just booting to Ubuntu that's all.

FTF is referring Yocto Project. But Yocto project is not for Ubuntu. is Ubuntu be built using Yocto project. if So, How.

is there anyway we can get Ubuntu Souce and build it for IMx6DL board. How???

How to get SD  card image files (.img/.sdcard) from Source.

Labels (4)
0 Kudos
1 Reply

709 Views
igorpadykov
NXP Employee
NXP Employee

HI Srinivasa

ubuntu sources are provided by The leading OS for PC, tablet, phone and cloud | Ubuntu

Re: iMX53 Quick Start Board - The origin of the MicroSD - Ubuntu 10.04 (Lucid) for ARM

for bulding for i.MX6 one can look at below

i.MX6q SABRE Board for Smart Devices - Linux on ARM - eewiki

http://boundarydevices.com/trusty-ubuntu-mx6/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos