How to run USB Host compliance test in iMX280

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run USB Host compliance test in iMX280

571 Views
ranjananaik
Contributor I

Hi All,

We are using the iMx280 in our product and would like to run the USB Host port compliance for the same.

By modifying the USBCMD(80090140) and PTC bits of PORTSC1(80090184) registers, we are able to run the J, K, SE0 and Test Packet.

For running the other tests on the compliance test suite, (Host Controller Packet Parameters , Host Disconnect Detect,  Host Suspend/Resume Timing), what are the commands or the instruction flow to generate the required patterns.

Regards,

Ranjana

0 Kudos
1 Reply

412 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Ranjana,

Could you please specify which BSP are you using? Have you checked the following thread which seems to be a similar case using Windows CE 6.0 BSP?

i.MX28 Accessing USB Test Modes Windows CE 6.0

Hope this will be useful for your.

Best regards!

/Carlos

0 Kudos