Different Display Configurations on the i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Different Display Configurations on the i.MX6

784 Views
osmarfrisonjun1
Contributor III

>> SABRE-SD iMX 6Quad

>> Linux 3.14.28 + yocto

>> Display LG LB070WV8 7.0”W (800 X 480) - LVDS

The goal is to port the Display mentioned to the SABRE-SD. There is an AN that explains how to do this to the i.MX6?

Thanks.

Labels (4)
Tags (2)
0 Kudos
1 Reply

431 Views
igorpadykov
NXP Employee
NXP Employee

Hi osmarfrisonjunior

background is described in

AN3974 Different Display Configurations on i.MX35 Linux PDK

some examples can be found on

i.MX6Q LVDS Wrong clock issue

how to support WSVGA output in imx6sdq

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos