ubuntu12.04 install ltib Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ubuntu12.04 install ltib Error

579 Views
shanfeifei
Contributor II

the err shows that:

ss@ubuntu:~/shanyf/P4080-PCIE-SDK-1.0-05-03-2012/ltib-e500mc-20110415$ ./ltib

Installing host support packages.

This only needs to be done once per host, but may take up to
an hour to complete ...

If an error occurs, a log file with the full output may be found in:
/home/shanyf/shanyf/P4080-PCIE-SDK-1.0-05-03-2012/ltib-e500mc-20110415/host_config.log

Exiting on error or interrupt
Please see >> /home/shanyf/shanyf/P4080-PCIE-SDK-1.0-05-03-2012/ltib-e500mc-20110415/host_config.log for details

the host_config.log shows that:

rpmdb: --force-debian: unknown option

Died at ./ltib line 2339.

traceback:

main::setup_rpmdb:2339

  main::check_rpm_setup:2403

   main::host_checks:1424

    main:543

Started: Thu Jul 16 18:54:40 2015

Ended:   Thu Jul 16 18:54:41 2015

Elapsed: 1 seconds

help me,what should i do ,thanks

Labels (1)
0 Kudos
1 Reply

305 Views
alexander_yakov
NXP Employee
NXP Employee

This question is frequently asked, for example please look this topic:

LTIB on Ubuntu 12.04

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos