Trying to Bring up Kernel
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.14.28_1.0.0_ga.
After Uboot logs I dint find any Kernel Logs then I implemented my own putc inside misc.c function to check whether uncompression linux is happening or not.
Uncompressing Linux... done, booting the kernel
I got the logs. But after that I am not able to get any early print logs.
Note:- I have enabled CONFIG_DEBUG_LL and EARLY_PRINTK.
CONFIG_DEBUG_LL=y
CONFIG_DEBUG_IMX_UART_PORT=2
CONFIG_DEBUG_LL_INCLUDE="mach/debug-macro.S"
CONFIG_UNCOMPRESS_INCLUDE="debug/uncompress.h"
CONFIG_EARLY_PRINTK=y
With the current definitions, I am able to see early print logs in 3.10 Kernel which i am running now on my board.
Kindly Suggest if i am missing out anything.
Solved! Go to Solution.
The link you shared is also same link which is shared by me.
This problem is solved now.
Found CONFIG_DEBUG_IMX_UART_PORT is configured to wrong Port no 1 i.e ttymxc0. After configuring it to 2 (ttymxc1) which we passed from Uboot. I could see early print logs after that.
Just for reference I'm adding a link to a very similar thread with more information on this:
The configuration looks fine. Are you still having this issue?
The link you shared is also same link which is shared by me.
This problem is solved now.
Found CONFIG_DEBUG_IMX_UART_PORT is configured to wrong Port no 1 i.e ttymxc0. After configuring it to 2 (ttymxc1) which we passed from Uboot. I could see early print logs after that.