I'm on a Mac, and was hoping to run my debugger in eclipse via OpenOCD CMSIS DAP interface.
I installed the OpenOCD package (0.9) from The GNU ARM Eclipse OpenOCD | GNU ARM Eclipse
and installed the corresponding eclipse plugin in KDS.
When I run the hello example, I get the error unable to find the kinetis.cfg file. Erich Styger provided the config file in another chain, and I also installed KDS on my PC and pulled the file from there (thinking that maybe newer).
In any case, I then copied the file to /Applications/GNU ARM Eclipse/OpenOCD/0.9.0-201505191004/scripts
Now when I run it, I get the error:
/Applications/GNU ARM Eclipse/OpenOCD/0.9.0-201505191004//scripts/kinetis.cfg:11: Error: invalid subcommand "newdap kinetis cpu -irlen 4"
in procedure 'script'
at file "embedded:startup.tcl", line 60
in procedure 'cmsis-dap' called at file "/Applications/GNU ARM Eclipse/OpenOCD/0.9.0-201505191004//scripts/kinetis.cfg", line 11
Does anyone have a solution?
Hi Raj,
Please take a look to Joe's answer on your other post:
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer