IMX6DL has ipu_warning!!!IPU_INT_STAT_10 /IPU_INT_STAT_5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL has ipu_warning!!!IPU_INT_STAT_10 /IPU_INT_STAT_5

2,991 Views
尚飞汤
Contributor IV

IPU Warning - IPU_INT_STAT_10 = 0x00080000

DI0 Synchronous display error interrupt

This bit indicates on the interrupt that is a result of an error during access to a synchronous display via DI0

IPU Warning - IPU_INT_STAT_5 = 0x00800000

New Frame before end-of-frame error indication of Channel interrupt. This bit is the status bit of New

Frame before end-of-frame error interrupt of Channel #n.

n Indicates the corresponding DMA channel number.

0 Interrupt is cleared.

1 Interrupt is requested.

however,i cannot decice what leads to this warning.can anyone help to tell me what config maybe connected with this warning???

Labels (1)
Tags (2)
0 Kudos
14 Replies

1,600 Views
Yuri
NXP Employee
NXP Employee

  Please refer to the following.

What does imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 mean?


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,600 Views
尚飞汤
Contributor IV

hai,yuri,I reduce the frame rate from 60 to 50,but it is not work ok.

0 Kudos

1,600 Views
Yuri
NXP Employee
NXP Employee

It is needed to consider the system in whole - perhaps the system is overloaded.

Regards,

Yuri.

0 Kudos

1,600 Views
尚飞汤
Contributor IV

well,i see there has a patch for the IPU_INT_STAT_5 = 0x00800000,does it suit my problem?

by the way ,we have usb and ethernet/bt/wifi, have no camera.

at the same time,the BT and wifi ethernet is no connect with ipu, how can that affect my display moudle?????

0 Kudos

1,600 Views
Yuri
NXP Employee
NXP Employee

Please refer to Qiang Li reply :


Re: i.MX6 Warning IPU_INT_STAT_10 = 0x00080000

Regards,

Yuri.

0 Kudos

1,600 Views
尚飞汤
Contributor IV

Dear yuri,i have try this ,but it is not work,there still have ipu warning.

0 Kudos

1,600 Views
Yuri
NXP Employee
NXP Employee

If You use one display, You can add "dmfc=3" in kernell boot command line.

This can let the single display use all of the DMFC FIFO.

Regards,

Yuri.

0 Kudos

1,600 Views
尚飞汤
Contributor IV

dear yuri,i have add it to the cmd,but there still have the warning.but still thank you for your help.

0 Kudos

1,600 Views
Yuri
NXP Employee
NXP Employee

You may try using recent BSP(s).

Regards,

Yuri.

0 Kudos

1,600 Views
尚飞汤
Contributor IV

Dear yuri:

how to try the new bsp?will it have a lot change?

0 Kudos

1,600 Views
Yuri
NXP Employee
NXP Employee

  You may find demo images (.sdcard fime extention), such as

" fsl-image-gui-x11-imx6qdlsolo.sdcard" for the recent BSP (L3.14.28)

in the following bundle.

  http://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_iMX6QDLS_BUNDLE

Please use the next Linux command to copy it to SD card :

$ sudo dd if= ./fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb bs=1M

0 Kudos

1,600 Views
尚飞汤
Contributor IV

Dear yuri,I the bsp download always fail,i will try again,

but something confuse me:

our project use mfg tool to download,i want to know what the relationship of boot.img and BSP?

in fact,maybe we have different called about bsp. can you tell me what the meaning of your meaning about BSP?

0 Kudos

1,600 Views
Yuri
NXP Employee
NXP Employee

   I meant, You may prepare boot SD card under host Linux :

$ sudo dd if= ./fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb bs=1M

Regards,

Yuri.

0 Kudos

1,600 Views
尚飞汤
Contributor IV

Dear yuri  :

我发现15寸的有这个问题,但是七寸和十寸的都没有这样的问题。

如果使用最新的BSP是否会涉及很多改动?我司这边项目已经进行到了一半了

Best regards

0 Kudos