can we create MQX project for TWR_K61 board using KDS_2.0.0 and KSDK_1.1.0 and MQX 4.1 ?
I couldn't find any k61 option in KDS .
Hello Joseph,
you can create your project with MQX 4.1. using KDS 2.0. but without KSDK.
the KSDK support for K60D10 series you can read from fsl_device_registers.h
#elif (defined(CPU_MK60DN256VLL10) || defined(CPU_MK60DX256VLL10) || defined(CPU_MK60DN512VLL10) || \
defined(CPU_MK60DN256VLQ10) || defined(CPU_MK60DX256VLQ10) || defined(CPU_MK60DN512VLQ10) || \
defined(CPU_MK60DN256VMC10) || defined(CPU_MK60DX256VMC10) || defined(CPU_MK60DN512VMC10) || \
defined(CPU_MK60DN256VMD10) || defined(CPU_MK60DX256VMD10) || defined(CPU_MK60DN512VMD10))
You can see there is no support for your MCU.
Best Regards,
Iva
How can we create MQX project for TWR_K61 board using KDS_2.0.0 and MQX 4.1 ?
Can u explain in detail with steps that I should follow.
Is there any cpp example for twrk22 board using KDS_2.0.0 and KSDK_1.1.0?where can I find it ?
Can we run cpp code using KDS_2.0.0 and KSDK_1.1.0?
Hello josephxavier,
Sure. For KSDK 1.1. you can look at demo C:\Freescale\KSDK_1.1.0\demos\hello_world\kds which is for twrk22f120m and twrk22f120mk02.
But I can recommend you to use new version for KSDK 1.2. and KDS 3.0.
New Kinetis Design Studio V3.0.0 available
for KSDK 1.2. is located C:\Freescale\KSDK_1.2.0\examples\twrk22f120m\demo_apps\flash_demo\kds
and example with MQX at C:\Freescale\KSDK_1.2.0\rtos\mqx\mqx\examples\mutex\build\kds\mutex_twrk22f120m
Best Regards,
Iva
Can u explain ?
With steps I am new to KDS 2.0 AND KSDK
Hi josephxavier,
KSDK does not support all devices. So it is better to find out if your device is supported.
Information about supported devices you can find at Release Note and in addition you can read it for more details from the fsl_device_registers.h which is located in your KSDK folder.
If you are new in KDS and KSDK
Please, start with Getting Started with Kinetis Design Studio, - it is IDE for Kinetis devices. But I recommend to wait 2-3 days for new version of KSDK and KDS.
http://cache.freescale.com/files/soft_dev_tools/doc/support_info/KSDKGSUG.pdf
Here you can download KSDK from websites Software Development Kit for Kinetis MCUs|Freescale
After installation, please go to folder C:\Freescale\KSDK_1.2.0\doc there is a lot of documentation which can help you start with programming MCUs.
Getting Started with Kinetis SDK (KSDK).pdf is document which you should start.
I think the best way is to try demos, which KSDK offeres.
You can find it e.g. C:\Freescale\KSDK_1.2.0\apps\frdmk64f\demos
with documentation Kinetis SDK v.1.2 Demo Applications User's Guide_review.pdf or at C:\Freescale\KSDK_1.2.0\doc\Kinetis SDK v.1.2 Demo Applications User's Guide is html page.
and I can recommend you following links
Can this help?
Iva
Hello joseph,
You can create project only with MQX 4.1. because there is no support for KSDK.
There is no support for current KSDK 1.1.0. But we plan it in future.
For only MQX 4.1. is support for TWR-K60F120M.
In KDS you can work with Processors > MK60 > MK61F
Hope this helps,
Iva
can we create MQX project for TWR_K61 board using KDS_2.0.0 and KSDK_1.1.0
Hi Josephxavier,
I am sorry, but current KSDK hasn't support Kinetis 120MHz/150MHz parts yet, which would be supported in the future.
Have a great day!
Kan