hello Community.
My host environment is Ubuntu 14.04.2 LTS 64bit.
Target board is using the i.MX6QSABRE Lite board.
Refer to the links in the community has seen progress the yocto Project.
i.MX Yocto Project: How Can I Build the Freescale Yocto Images using bitbake?
However, the following problems occurred.
lite@Q:~/fsl-community-bsp/build/tmp/deploy/images/imx6qsabrelite$ df -h
(I changed the SD card formatted with NTFS.)
Filesystem Size Used Avail Use% Mounted on
/dev/sda1 222G 21G 190G 10% /
none 4.0K 0 4.0K 0% /sys/fs/cgroup
udev 1.9G 4.0K 1.9G 1% /dev
tmpfs 382M 1.2M 381M 1% /run
none 5.0M 0 5.0M 0% /run/lock
none 1.9G 156K 1.9G 1% /run/shm
none 100M 48K 100M 1% /run/user
/dev/sdb1 7.4G 62M 7.4G 1% /media/lite/04F28F7DF28F71AA
(imx6qsabrelite directory is 하드웨어 - imx6 YOCTO Project build was this refer to the link.)
lite@Q:~/fsl-community-bsp/build/tmp/deploy/images/imx6qsabrelite$ sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdb1
6+0 records in
6+0 records out
25165824 bytes (25 MB) copied, 0.0477638 s, 527 MB/s
----------------------------------------------------------
-> My sd card became the read-only.
After inserting the board but failed attempt to boot.
Switch this setting is that correct?
D1 SW= ON, D2 SW=OFF
I used two ways.
1) D1 SW= ON, D2 SW=OFF
2) D1 SW= OFF, D2 SW=OFF
...
The failed.:smileysad:
Is there any doubt part?
I hope the answer.:smileysilly:
thank you.
Solved! Go to Solution.
Hi,
Please try this:
sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdb
Best Regards,
Alejandro
Hi,
Please try this:
sudo dd if=core-image-minimal-imx6qsabrelite.sdcard of=/dev/sdb
Best Regards,
Alejandro
Hi,
Thank you for your post, however please consider moving it to the right community place for better visibility.
For details please see general advice https://community.freescale.com/docs/DOC-99909
/Alejandro