We now use a board based on MCF54418,and its circuit is the same as development board(TWR-MCF5441x (700-26131))bought from freescale。The NAND flash is 16bit IC MT29F2G16AADWP . But now,we want change NAND flash to 8bit MT29F2G08ABAEAWP‐IT because of its lifecycle.
About the code , i have just change "#define MT29F2G16_WIDTH 16" to "8" in MT29F2G16.c as below. But it does not work.
So I am very confused for a long time. Is there anything else should be change?
Hello Eric,
Please check my answer in the thread Re: MCF54418 Use 8bit NAND flash failed
and let me know if this helps!!
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------