Hi m.c
Was it useful the Community thread mentioned by Saurabh? Did you was able to rotate the screen?
Best regards!
/Carlos
It can rotate 180 degree by user land program from Saurabh suggestion. However, customer needs rotate display in the begining when boot. If screen frame buffer can rotate in operating system level, the graphic application doesn't need modify anything. Can i.MX53 Linux support display rotate 180 degree in OS level?
Hi m.c
It seems that in the following thread they are also asking about rotate the screen during boot time, so you could try these implementations:
https://community.freescale.com/message/304789
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------