TWRVF65GS10:I2S slave mode configuration issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWRVF65GS10:I2S slave mode configuration issue

Jump to solution
1,912 Views
manjug
Contributor III

Hi,

I'm configuring I2S as receive slave for receiving audio from source which provides Bitclock ,Wordsync and raw audio. I'm using DMA based data transfer.Using MQX RTOS.

Below is my configuration code:

_mqx_int init_I2S()

{

    _mqx_int  errcode = 0;

    _mqx_int    param = 0;// temp;

    char* modeString = NULL;

    MQX_FILE_PTR i2s_ptr = NULL;

     _mqx_uint type=IO_IOCTL_I2S_SET_MODE_SLAVE;

    uint8_t mode = (I2S_RX_MASTER | I2S_RX_SLAVE);

    I2S_STATISTICS_STRUCT stats;

    AUDIO_DATA_FORMAT audio_format;

    audio_format.ENDIAN = AUDIO_LITTLE_ENDIAN;

    audio_format.ALIGNMENT = AUDIO_ALIGNMENT_LEFT;

    audio_format.BITS = 32;

    audio_format.SIZE = 1;

    audio_format.CHANNELS = 2;

 

      if ((i2s_ptr = fopen("sai:", NULL)) == NULL)

    {

        printf("  Error: Unable to open a device \n");

        return ;

    }

   

    printf("I2S Open Success\n");

    result = ioctl(i2s_ptr, type, &mode);

    if(result==I2S_OK)

    {

     printf("Mode Success\n");

    }

    else

    {

     printf("Mode Error = %02x\n",result);

    }

    if (ioctl(i2s_ptr, IO_IOCTL_AUDIO_SET_IO_DATA_FORMAT, &audio_format) != I2S_OK)

    {

        printf("  Error: Input data format not supported.\n");

        fclose(i2s_ptr);

    }

    }

I'm using PTB0(SAI2_RX_BCLK),PTB1(SAI2_RX_DATA), and PTB2(SAI2_RX_SYNC).J8 header pin 38,39 and 40.

Below is the init_gpio.c code :

_mqx_int _bsp_sai_io_init

(

    _mqx_uint dev_num

)

{

    switch(dev_num)

    {

        case 0: // SAI0

            CCM_CSCMR1 = (CCM_CSCMR1 & ~CCM_CSCMR1_SAI0_CLK_SEL_MASK) | CCM_CSCMR1_SAI0_CLK_SEL(3);

            CCM_CSCDR1 = (CCM_CSCMR1 & ~CCM_CSCDR1_SAI0_DIV_MASK) | CCM_CSCDR1_SAI0_DIV(0x0f);

            CCM_CSCDR1 |= CCM_CSCDR1_SAI0_EN_MASK;

            // RX_BCLK

            //IOMUXC_SW_MUX_CTL_PAD_PAD_11 = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

            // RX_DATA

            //IOMUXC_SW_MUX_CTL_PAD_PAD_12 = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

            // RX_SYNC

            //IOMUXC_SW_MUX_CTL_PAD_PAD_13 = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

            // TX_SYNC

            IOMUXC_RGPIO(98) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_DSE(7) |

                IOMUXC_SW_MUX_CTL_PAD_PAD_PUS(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_PKE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_PUE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_OBE_MASK;

            // TX_DATA

            IOMUXC_RGPIO(96) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_DSE(7) |

                IOMUXC_SW_MUX_CTL_PAD_PAD_PUS(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_PKE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_PUE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_OBE_MASK;

            // TX_BCLK

            IOMUXC_RGPIO(93) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_DSE(7) | \

                IOMUXC_SW_MUX_CTL_PAD_PAD_PUS(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_PKE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_PUE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_OBE_MASK;

            break;

        case 2:

            // RX_DATA PTB1

            IOMUXC_RGPIO(23) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

            /*Daisy chain Selecting Pad: PTB1 for Mode: ALT5 (SAI2_RX_DATA)*/

            IOMUXC_SAI2_IPP_IND_SAI_RXDATA_0_SELECT_INPUT = 0x01;

// SAI2_RX_BCLK PTB0

  IOMUXC_RGPIO(22) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

  /*Daisy chain Selecting Pad: PTB0 for Mode: ALT5 (SAI2_RX_BCLK)*/

  IOMUXC_SAI2_IPP_IND_SAI_RXBCLK_SELECT_INPUT = 0x01;

  // SAI2_RX_SYNC PTB2

  IOMUXC_RGPIO(24) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

  /*Daisy chain Selecting Pad: PTB2 for Mode: ALT5 (SAI2_RX_SYNC)*/

  IOMUXC_SAI2_IPP_IND_SAI_RXSYNC_SELECT_INPUT = 0x01;

            // RX_DATA

            IOMUXC_RGPIO(23) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

           /*Daisy chain Selecting Pad: PTB1 for Mode: ALT5 (SAI2_RX_DATA)*/

            IOMUXC_SAI2_IPP_IND_SAI_RXDATA_0_SELECT_INPUT = 0x01;

            // RX_SYNC

            IOMUXC_RGPIO(13) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;

            break;

        default:

            break;

    }

    return MQX_OK;

}

When i start receving using DMA mode it hangs at   ioctl(i2s_ptr, IO_IOCTL_I2S_WAIT_RX_EVENT, NULL);

Labels (2)
1 Solution
1,519 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
5 Replies
1,520 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
1,522 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Just as reference, the question Rene and Naoum  refer to is this one:

Re: I2s capture in vybrid is noisy

Regards,

Alejandro

0 Kudos
1,522 Views
rendy
NXP Employee
NXP Employee

Hi Manju,

  1. There's a duplicate question created by you here: TWRVF65GS10:I2S slave configuration issue. It's marked as answered, is it correct? Did you check the link there as suggested by Naoum? Did it help you?
  2. In case your problem persists:
    1. What's your MQX version
    2. What's the board

Rene

1,522 Views
cyborgnegotiato
Senior Contributor II

rendy could you look at it?

Thanks,

Jozef

1,522 Views
naoumgitnik
Senior Contributor V

Duplicate of TWRVF65GS10:I2S slave configuration issue; karinavalencia, may you delete it, please?

Below is what I replied there with:

"Have you looked at the Re: I2s capture in vybrid is noisy thread, please?

It looks like the problem is different in that thread than yours and most likely not related to the I2S interface; therefore, quite likely the approach  and settings used there might work for you."

Thanks, Naoum Gitnik.

0 Kudos