Hi,
I'm configuring I2S as receive slave for receiving audio from source which provides Bitclock ,Wordsync and raw audio. I'm using DMA based data transfer.Using MQX RTOS.
Below is my configuration code:
_mqx_int init_I2S()
{
_mqx_int errcode = 0;
_mqx_int param = 0;// temp;
char* modeString = NULL;
MQX_FILE_PTR i2s_ptr = NULL;
_mqx_uint type=IO_IOCTL_I2S_SET_MODE_SLAVE;
uint8_t mode = (I2S_RX_MASTER | I2S_RX_SLAVE);
I2S_STATISTICS_STRUCT stats;
AUDIO_DATA_FORMAT audio_format;
audio_format.ENDIAN = AUDIO_LITTLE_ENDIAN;
audio_format.ALIGNMENT = AUDIO_ALIGNMENT_LEFT;
audio_format.BITS = 32;
audio_format.SIZE = 1;
audio_format.CHANNELS = 2;
if ((i2s_ptr = fopen("sai:", NULL)) == NULL)
{
printf(" Error: Unable to open a device \n");
return ;
}
printf("I2S Open Success\n");
result = ioctl(i2s_ptr, type, &mode);
if(result==I2S_OK)
{
printf("Mode Success\n");
}
else
{
printf("Mode Error = %02x\n",result);
}
if (ioctl(i2s_ptr, IO_IOCTL_AUDIO_SET_IO_DATA_FORMAT, &audio_format) != I2S_OK)
{
printf(" Error: Input data format not supported.\n");
fclose(i2s_ptr);
}
}
I'm using PTB0(SAI2_RX_BCLK),PTB1(SAI2_RX_DATA), and PTB2(SAI2_RX_SYNC).J8 header pin 38,39 and 40.
Below is the init_gpio.c code :
_mqx_int _bsp_sai_io_init
(
_mqx_uint dev_num
)
{
switch(dev_num)
{
case 0: // SAI0
CCM_CSCMR1 = (CCM_CSCMR1 & ~CCM_CSCMR1_SAI0_CLK_SEL_MASK) | CCM_CSCMR1_SAI0_CLK_SEL(3);
CCM_CSCDR1 = (CCM_CSCMR1 & ~CCM_CSCDR1_SAI0_DIV_MASK) | CCM_CSCDR1_SAI0_DIV(0x0f);
CCM_CSCDR1 |= CCM_CSCDR1_SAI0_EN_MASK;
// RX_BCLK
//IOMUXC_SW_MUX_CTL_PAD_PAD_11 = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;
// RX_DATA
//IOMUXC_SW_MUX_CTL_PAD_PAD_12 = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;
// RX_SYNC
//IOMUXC_SW_MUX_CTL_PAD_PAD_13 = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;
// TX_SYNC
IOMUXC_RGPIO(98) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_DSE(7) |
IOMUXC_SW_MUX_CTL_PAD_PAD_PUS(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_PKE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_PUE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_OBE_MASK;
// TX_DATA
IOMUXC_RGPIO(96) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_DSE(7) |
IOMUXC_SW_MUX_CTL_PAD_PAD_PUS(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_PKE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_PUE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_OBE_MASK;
// TX_BCLK
IOMUXC_RGPIO(93) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_DSE(7) | \
IOMUXC_SW_MUX_CTL_PAD_PAD_PUS(1) | IOMUXC_SW_MUX_CTL_PAD_PAD_PKE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_PUE_MASK | IOMUXC_SW_MUX_CTL_PAD_PAD_OBE_MASK;
break;
case 2:
// RX_DATA PTB1
IOMUXC_RGPIO(23) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;
/*Daisy chain Selecting Pad: PTB1 for Mode: ALT5 (SAI2_RX_DATA)*/
IOMUXC_SAI2_IPP_IND_SAI_RXDATA_0_SELECT_INPUT = 0x01;
// SAI2_RX_BCLK PTB0
IOMUXC_RGPIO(22) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;
/*Daisy chain Selecting Pad: PTB0 for Mode: ALT5 (SAI2_RX_BCLK)*/
IOMUXC_SAI2_IPP_IND_SAI_RXBCLK_SELECT_INPUT = 0x01;
// SAI2_RX_SYNC PTB2
IOMUXC_RGPIO(24) = IOMUXC_SW_MUX_CTL_PAD_PAD_MUX_MODE(5) | IOMUXC_SW_MUX_CTL_PAD_PAD_IBE_MASK;
/*Daisy chain Selecting Pad: PTB2 for Mode: ALT5 (SAI2_RX_SYNC)*/
IOMUXC_SAI2_IPP_IND_SAI_RXSYNC_SELECT_INPUT = 0x01;
break;
default:
break;
}
return MQX_OK;
}
When i start receving using DMA mode it hangs at ioctl(i2s_ptr, IO_IOCTL_I2S_WAIT_RX_EVENT, NULL);
Dear Manju,
I know it is an old question, since not closed, were you able to identify the issue ? We are facing a similar failure mode.
Gabriel
Dear Manju,
Have you looked at the Re: I2s capture in vybrid is noisy thread, please?
It looks like the problem is different in that thread than yours and most likely not related to the I2S interface; therefore, quite likely the approach and settings used there might work for you.
Sincerely, Naoum Gitnik.