Hello
I suffered a problem in android 4.4.2 with mx6q_sabresd custom board. That is when I put finger in the screen ,then the cursor appeared just like you use the mouse. When I put the finger in the middle of touch screen, the mouse overlaps with finger, in the other hand, it is very accuracy in the middle of screen. Unfortunately, I move the finger to the left of edge of screen , the mouse is right to the finger, then I move the finger to the right of edge of screen , the mouse is left the finger, and at last I move the finger to the down of edge of screen, the mouse is up to finger. It looks like the panel smaller than touch screen. It is very not accuracy around the touch. I doubt that the mouse cursor make touch screen not accuracy, because I find eGalax_Touch_Screen.idc file in system/usr/idc/ , the contents tell us it doesn't need to calibrate.
===========================
cat /proc/bus/input/devices
..
..
Handlers= mouse event3
..
..
===========================
eGalax_Touch_Screen.idc
touch.deviceType = touchScreen
touch.orientationAware = 1
touch.size.calibration = none
touch.orientation.calibration = none
=============================
1 Is my guess accurate?
2 How can I remove the mouse when I put finger in the screen?
3 How can I verify that idc file is loaded accurately?
4 If my guess is wrong. What method to let me calibrate? tslib ? I have porting tslib in Android 4.4 and get 7 coefficients but I don't know
how to apply them.
ps. kernel driver for touch screen is egalax_ts.c. I need to revise it ?
Thanks very much.
Hi Bernie
usually calibration information is stored on:
/media/data/system/calibration
To replace this data one needs to add “calibration” at the bootup command line.
In case this does not trigger the calibration when rebooting, one can try removing this
file. After rebooting it should initiate calibration.
Resistive Touchscreen Calibration Program on iMX6Q with Android ICS 4.0.4
http://forum.xda-developers.com/showthread.php?t=2263582
Best regards
igor