hi all this is saida
i am starting design based i.mx processor
i have some doughts
1. can i place solo processor on Dual lite based evalution board which i have taken reference for design
2. in dual lite can i enable only one core for processing and single DDR is sufficient or not
3. is two cores can share a single DDR
thank you in advance
Hi saida
yes, one can place solo processor on Dual lite based evalution board.
In dual lite one can enable only one core for processing, single DDR is sufficient.
Two cores can share a single DDR.
Also it may be useful to look at AN4397
Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
First of all i thank mr Igor for his valuable reply
i am new bee for i.mx6 DualLite processor and want to design new
custom made board
my requirement is i want to start a new board and ready to purchase
tools everything that processor needs
Design:
Host is Windows based PC
1. i want to design a new custom made board
2. i have to port U-boot for my board where i can store in Flash
3. i want to develop a non OS or OS approach code for my application
4. what are the IDE tools for code,compile.build,downloading,debugging
and flash programming
5. also i want hardware emulator(ICE) for my board .
kindly help me in this regard
Regards & Thanks
Saida Safavath