Wandboard Quad Yocto fsl-image-multimedia X server seg fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wandboard Quad Yocto fsl-image-multimedia X server seg fault

Jump to solution
1,960 Views
abhayghatpande
Contributor III

Hello Otavio,

I've seen you help a lot of people on the forums. Hope you can give me some advice too.


I built the fsl-image-multimedia for Wandboard Quad without problems. Also modified the u-boot arguments to change the resolution to 1920x1080@60M. The resolution is correctly detected by the X server. But the server seg faults and I'm unable to reach a tty either. I'm only able to send you a partial Xorg.0.log file because am unable to transfer it out of the board without ssh or some other mechanism.


Any idea what could be the reason? Is there any info that would help you debug?


Thanks,

Abhay


2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)

[3249511.052] (II) VIVANTE(0): Modeline "S:1280x720p-60"x0.0   74.25  1280 1390

1430 1650  720 725 730 750 +hsync +vsync -csync (45.0 kHz e)

[3249511.052] (II) VIVANTE(0): Modeline "S:720x480p-60"x0.0   27.00  720 736 798

858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.052] (II) VIVANTE(0): Modeline "S:720x480p-60"x0.0   27.00  720 736 798

858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.052] (II) VIVANTE(0): Modeline "S:640x480p-60"x0.0   25.17  640 656 752

800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.053] (II) VIVANTE(0): Modeline "V:640x480p-60"x0.0   25.20  640 656 752

800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.053] (II) VIVANTE(0): Modeline "D:1920x1080p-60"x0.0  148.50  1920 2008

2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz e)

[3249511.053] (II) VIVANTE(0): Modeline "V:640x480p-60"x0.0   25.20  640 656 752

800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.105] (II) VIVANTE(0): Output DISP3 BG has no monitor section

[3249511.105] (II) VIVANTE(0): Printing probed modes for output DISP3 BG

[3249511.105] (II) VIVANTE(0): Modeline "S:1920x1080p-60"x60.0  148.50  1920 200

8 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)

[3249511.105] (II) VIVANTE(0): Modeline "S:1920x1080p-50"x50.0  148.50  1920 244

8 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)

[3249511.105] (II) VIVANTE(0): Modeline "S:1280x720p-50"x50.0   74.25  1280 1720

1760 1980  720 725 730 750 +hsync +vsync -csync (37.5 kHz e)

[3249511.105] (II) VIVANTE(0): Modeline "S:1280x720p-60"x60.0   74.25  1280 1390

1430 1650  720 725 730 750 +hsync +vsync -csync (45.0 kHz e)

[3249511.105] (II) VIVANTE(0): Modeline "S:720x576p-50"x50.0   27.00  720 732 79

6 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[3249511.106] (II) VIVANTE(0): Modeline "S:720x480p-60"x59.9   27.00  720 736 79

8 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.106] (II) VIVANTE(0): Modeline "V:640x480p-60"x60.0   25.20  640 656 75

2 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.106] (II) VIVANTE(0): Modeline "S:640x480p-60"x59.9   25.17  640 656 75

2 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3249511.106] (II) VIVANTE(0): Output DISP3 BG connected

[3249511.106] (II) VIVANTE(0): Using exact sizes for initial modes

[3249511.106] (II) VIVANTE(0): Output DISP3 BG using initial mode S:1920x1080p-6

0

[3249511.106] (II) VIVANTE(0): imxDisplayPreInit: virtual set 1920 x 1080, displ

ay width 0

[3249511.106] (II) VIVANTE(0): FBDevPreInit: adjust display width 1920

[3249511.106] (**) VIVANTE(0): PreInit done

[3249511.106] (--) Depth 24 pixmap format is 32 bpp

[3249511.106] (II) VIVANTE(0): Init mode for fb device

[3249511.198] (II) VIVANTE(0): hardware: DISP3 BG (video memory: 16335kB)

[3249511.199] (II) VIVANTE(0): FB Start = 0x75666000  FB Base = 0x75666000  FB O

ffset = (nil) FB PhyBase 0x76a00000

[3249511.199] (II) VIVANTE(0): reserve 8355840 bytes for on screen frame buffer;

total fb memory size 16727040 bytes; offset of shadow buffer 8355840

[3249511.273] (II) VIVANTE(0): hardware: DISP3 BG (video memory: 16335kB)

[3249511.290] (II) VIVANTE(0): test Initializing EXA

[3249511.290] (II) VIVANTE(0): (driver build from: -dirty)

[3249511.291] (II) EXA(0): Driver allocated offscreen pixmaps

[3249511.291] (II) EXA(0): Driver registered support for the following operation

s:

[3249511.291] (II)         Solid

[3249511.291] (II)         Copy

[3249511.291] (II)         Composite (RENDER acceleration)

[3249511.291] (II)         UploadToScreen

[3249511.291] (EE)

[3249511.291] (EE) Backtrace:

[3249511.291] (EE)

[3249511.292] (EE) Segmentation fault at address 0xd8

[3249511.292] (EE)

Fatal server error:

[3249511.292] (EE) Caught signal 11 (Segmentation fault). Server aborting

[3249511.292] (EE)

[3249511.292] (EE)

Please consult the The X.Org Foundation support

         at http://wiki.x.org

for help.

[3249511.292] (EE) Please also check the log file at "/var/log/Xorg.0.log" for a

dditional information.

[3249511.292] (EE)

[3249511.387] (EE) Server terminated with error (1). Closing log file.

Tags (2)
1 Solution
1,046 Views
OtavioSalvador
Senior Contributor II

Master has been updated to 3.10.31 BSP and  thus the Wandboard needs update to match the BSP kernel and GPU drivers.         

View solution in original post

0 Kudos
7 Replies
1,046 Views
abhayghatpande
Contributor III

So it seems to be something to do with the EXA driver since the error pops up once it's loaded.

Some seg faults with EXA have been reported: iMX6Q / Yocto: X11 unstable (SIGSEGV) with acceleration enabled.

0 Kudos
1,046 Views
abhayghatpande
Contributor III

I changed the branch to dizzy and built fsl-image-multimedia-full again and voila!, X started up without any issues at all. So looks like something's broken in the master branch. It's too bad because I wanted to get the gstreamer-1.0 and audio.

Right now there is no audio playing (I did check using alsamixer), but that is for another discussion.

1,047 Views
OtavioSalvador
Senior Contributor II

Master has been updated to 3.10.31 BSP and  thus the Wandboard needs update to match the BSP kernel and GPU drivers.         

0 Kudos
1,046 Views
abhayghatpande
Contributor III

Thank you, Otavio. I switched to dizzy branch for now.

1,046 Views
abhayghatpande
Contributor III

Just FYI, during the build process, the following messages were generated.

WARNING: QA Issue: libfslcodec-test-bin rdepends on imx-vpu, but it isn't a build dependency? [build-deps]

WARNING: QA Issue: libg2d rdepends on libgal-mx6, but it isn't a build dependency? [build-deps]

WARNING: QA Issue: ELF binary '/home/abhay/fsl-community-bsp/build/tmp/work/cort

exa9hf-vfp-neon-poky-linux-gnueabi/libav/0.8.15-r0/packages-split/libavcodec/usr

/lib/libavcodec.so.53.35.0' has relocations in .text [textrel]

WARNING: QA Issue: ELF binary '/home/abhay/fsl-community-bsp/build/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/chromium/38.0.2125.101-r0/packages-spl

it/chromium/usr/bin/chrome/libffmpegsumo.so' has relocations in .text [textrel]WARNING: QA Issue: chromium-dbg: found library in wrong location: /usr/bin/chrom

e/.debug/libffmpegsumo.so

chromium: found library in wrong location: /usr/bin/chrome/libffmpegsumo.so [libdir]

WARNING: log_check: There is a warn message in the logfileWARNING: log_check: Matched keyword: [warn]

WARNING: log_check: warning: Schema 'org.freedesktop.gstreamer-0.10.default-elements' has path '/desktop/gstreamer/0.10/default-elements/'.  Paths starting with '/apps/', '/desktop/' or '/system/' are deprecated.

NOTE: Tasks Summary: Attempted 5013 tasks of which 4533 didn't need to be rerun

and all succeeded.

Summary: There were 9 WARNING messages shown.

0 Kudos
1,046 Views
abhayghatpande
Contributor III

I forgot to mention that I'm using the fsl-community-bsp master branch.

I changed the default init level to 3 so that I can get a tty and make some modifications to test X server settings.  Why does the server not return to the tty after a seg fault?

I think I know the reason for the seg fault -- there is no twm, xterm or xclock built in the image.

Any ideas how the core X11 apps are to be added to the image?

0 Kudos
1,046 Views
abhayghatpande
Contributor III

Ok. So I added twm and xterm and xclock to the image and the result is still the same.

The only other thing missing I noticed are the fonts. Here is the Xorg.0.log.

[3290117.826]

X.Org X Server 1.15.1

Release Date: 2014-04-13

[3290117.826] X Protocol Version 11, Revision 0

[3290117.826] Build Operating System: Linux 3.10.23-xxxx-std-ipv6-64 x86_64

[3290117.826] Current Operating System: Linux wandboard-quad 3.10.17-1.0.1-wand

board+ga6e7fc5 #2 SMP PREEMPT Mon Nov 17 23:26:47 EST 2014 armv7l

[3290117.826] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 r

ootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24

[3290117.826] Build Date: 18 November 2014  12:41:26PM

[3290117.826] 

[3290117.826] Current version of pixman: 0.32.6

[3290117.827]   Before reporting problems, check http://wiki.x.org

        to make sure that you have the latest version.

[3290117.827] Markers: (--) probed, (**) from config file, (==) default setting

,

        (++) from command line, (!!) notice, (II) informational,

        (WW) warning, (EE) error, (NI) not implemented, (??) unknown.

[3290117.827] (==) Log file: "/var/log/Xorg.0.log", Time: Tue Nov 18 18:12:38 2

014

[3290117.832] (==) Using config file: "/etc/X11/xorg.conf"

[3290117.832] (==) Using system config directory "/usr/share/X11/xorg.conf.d"

[3290117.844] (==) No Layout section.  Using the first Screen section.

[3290117.844] (==) No screen section available. Using defaults.

[3290117.844] (**) |-->Screen "Default Screen Section" (0)

[3290117.844] (**) |   |-->Monitor "<default monitor>"

[3290117.850] (==) No device specified for screen "Default Screen Section".

        Using the first device section listed.

[3290117.850] (**) |   |-->Device "i.MX Accelerated Framebuffer Device"

[3290117.850] (==) No monitor specified for screen "Default Screen Section".

        Using a default monitor configuration.

[3290117.850] (**) Option "BlankTime" "0"

[3290117.850] (**) Option "StandbyTime" "0"

[3290117.850] (**) Option "SuspendTime" "0"

[3290117.850] (**) Option "OffTime" "0"

[3290117.850] (==) Automatically adding devices

[3290117.850] (==) Automatically enabling devices

[3290117.850] (==) Automatically adding GPU devices

[3290117.858] (WW) The directory "/usr/share/fonts/X11/misc/" does not exist.

[3290117.858]   Entry deleted from font path.

[3290117.858] (WW) The directory "/usr/share/fonts/X11/TTF/" does not exist.

[3290117.858]   Entry deleted from font path.

[3290117.858] (WW) The directory "/usr/share/fonts/X11/OTF/" does not exist.

[3290117.858]   Entry deleted from font path.

[3290117.859] (WW) The directory "/usr/share/fonts/X11/Type1/" does not exist.

[3290117.859]   Entry deleted from font path.

[3290117.859] (WW) The directory "/usr/share/fonts/X11/100dpi/" does not exist.

[3290117.859]   Entry deleted from font path.

[3290117.859] (WW) The directory "/usr/share/fonts/X11/75dpi/" does not exist.

[3290117.859]   Entry deleted from font path.

[3290117.859] (==) FontPath set to:

[3290117.859] (==) ModulePath set to "/usr/lib/xorg/modules"

[3290117.859] (II) The server relies on udev to provide the list of input devic

es.

        If no devices become available, reconfigure udev or disable AutoAddDevi

ces.

[3290117.869] (II) Loader magic: 0x1aea88

[3290117.869] (II) Module ABI versions:

[3290117.869]   X.Org ANSI C Emulation: 0.4

[3290117.869]   X.Org Video Driver: 15.0

[3290117.869]   X.Org XInput driver : 20.0

[3290117.869]   X.Org Server Extension : 8.0

[3290117.870] (II) xfree86: Adding drm device (/dev/dri/card0)

[3290117.870] Initializing built-in extension Generic Event Extension

[3290117.870] Initializing built-in extension SHAPE

[3290117.870] Initializing built-in extension MIT-SHM

[3290117.870] Initializing built-in extension XInputExtension

[3290117.870] Initializing built-in extension XTEST

[3290117.870] Initializing built-in extension BIG-REQUESTS

[3290117.870] Initializing built-in extension SYNC

[3290117.870] Initializing built-in extension XKEYBOARD

[3290117.870] Initializing built-in extension XC-MISC

[3290117.870] Initializing built-in extension XFIXES

[3290117.871] Initializing built-in extension RENDER

[3290117.871] Initializing built-in extension RANDR

[3290117.871] Initializing built-in extension COMPOSITE

[3290117.871] Initializing built-in extension DAMAGE

[3290117.871] Initializing built-in extension MIT-SCREEN-SAVER

[3290117.871] Initializing built-in extension DOUBLE-BUFFER

[3290117.871] Initializing built-in extension DPMS

[3290117.871] Initializing built-in extension Present

[3290117.871] Initializing built-in extension X-Resource

[3290117.871] Initializing built-in extension XVideo

[3290117.871] Initializing built-in extension XVideo-MotionCompensation

[3290117.871] Initializing built-in extension XFree86-VidModeExtension

[3290117.871] Initializing built-in extension XFree86-DGA

[3290117.871] Initializing built-in extension XFree86-DRI

[3290117.871] Initializing built-in extension DRI2

[3290117.871] (II) LoadModule: "glx"

[3290117.893] (II) Loading /usr/lib/xorg/modules/extensions/libglx.so

[3290117.904] (II) Module glx: vendor="X.Org Foundation"

[3290117.904]   compiled for 1.15.1, module version = 1.0.0

[3290117.904]   ABI class: X.Org Server Extension, version 8.0

[3290117.904] (==) AIGLX enabled

[3290117.904] Loading extension GLX

[3290117.904] (II) LoadModule: "vivante"

[3290117.905] (II) Loading /usr/lib/xorg/modules/drivers/vivante_drv.so

[3290117.910] (II) Module vivante: vendor="X.Org Foundation"

[3290117.910]   compiled for 1.15.1, module version = 1.0.0

[3290117.910]   Module class: X.Org Video Driver

[3290117.910]   ABI class: X.Org Video Driver, version 15.0

[3290117.910] Loading extension vivext

[3290117.910] (II) VIVANTE: driver for vivante fb: VivanteGC500, VivanteGC2100,

        VivanteGCCORE

[3290117.910] (--) using VT number 2

[3290117.950] (WW) Falling back to old probe method for vivante

[3290117.950] (II) Loading sub module "fbdevhw"

[3290117.950] (II) LoadModule: "fbdevhw"

[3290117.950] (II) Loading /usr/lib/xorg/modules/libfbdevhw.so

[3290117.952] (II) Module fbdevhw: vendor="X.Org Foundation"

[3290117.952]   compiled for 1.15.1, module version = 0.0.2

[3290117.952]   ABI class: X.Org Video Driver, version 15.0

[3290117.952] (II) VIVANTE(0): using default device

[3290117.952] (WW) VGA arbiter: cannot open kernel arbiter, no multi-card suppo

rt

[3290117.952] (II) VIVANTE(0): Device preferred mode 'fb0':S:1920x1080p-60

[3290117.952] (II) VIVANTE(0): Creating default Display subsection in Screen se

ction

        "Default Screen Section" for depth/fbbpp 24/32

[3290117.952] (==) VIVANTE(0): Depth 24, (==) framebuffer bpp 32

[3290117.952] (==) VIVANTE(0): RGB weight 888

[3290117.953] (==) VIVANTE(0): Default visual is TrueColor

[3290117.953] (==) VIVANTE(0): Using gamma correction (1.0, 1.0, 1.0)

[3290117.953] (**) VIVANTE(0): Option "fbdev" "/dev/fb0"

[3290117.953] (II) VIVANTE(0): checking modes against framebuffer device...

[3290117.953] (II) VIVANTE(0): checking modes against monitor...

[3290117.953] (II) VIVANTE(0): Use built in mode (bpp 32)

[3290117.953] (--) VIVANTE(0): Virtual size is 0x0 (pitch 0)

[3290117.953] (==) VIVANTE(0): DPI set to (96, 96)

[3290117.953] (II) Loading sub module "fb"

[3290117.953] (II) LoadModule: "fb"

[3290117.953] (II) Loading /usr/lib/xorg/modules/libfb.so

[3290117.962] (II) Module fb: vendor="X.Org Foundation"

[3290117.962]   compiled for 1.15.1, module version = 1.0.0

[3290117.962]   ABI class: X.Org ANSI C Emulation, version 0.4

[3290117.962] (II) Loading sub module "exa"

[3290117.962] (II) LoadModule: "exa"

[3290117.962] (II) Loading /usr/lib/xorg/modules/libexa.so

[3290117.968] (II) Module exa: vendor="X.Org Foundation"

[3290117.968]   compiled for 1.15.1, module version = 2.6.0

[3290117.968]   ABI class: X.Org Video Driver, version 15.0

[3290118.100] (II) VIVANTE(0): printing discovered frame buffer 'fb0' supported

modes:

[3290118.100] (II) VIVANTE(0): Modeline "S:1920x1080p-50"x0.0  148.50  1920 244

8 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)

[3290118.100] (II) VIVANTE(0): Modeline "S:1280x720p-50"x0.0   74.25  1280 1720

1760 1980  720 725 730 750 +hsync +vsync -csync (37.5 kHz e)

[3290118.101] (II) VIVANTE(0): Modeline "S:720x576p-50"x0.0   27.00  720 732 79

6 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[3290118.101] (II) VIVANTE(0): Modeline "S:720x576p-50"x0.0   27.00  720 732 79

6 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[3290118.101] (II) VIVANTE(0): Modeline "S:1920x1080p-60"x0.0  148.50  1920 200

8 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)

[3290118.101] (II) VIVANTE(0): Modeline "S:1280x720p-60"x0.0   74.25  1280 1390

1430 1650  720 725 730 750 +hsync +vsync -csync (45.0 kHz e)

[3290118.102] (II) VIVANTE(0): Modeline "S:720x480p-60"x0.0   27.00  720 736 79

8 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.102] (II) VIVANTE(0): Modeline "S:720x480p-60"x0.0   27.00  720 736 79

8 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.102] (II) VIVANTE(0): Modeline "S:640x480p-60"x0.0   25.17  640 656 75

2 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.102] (II) VIVANTE(0): Modeline "V:640x480p-60"x0.0   25.20  640 656 75

2 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.103] (II) VIVANTE(0): Modeline "D:1920x1080p-60"x0.0  148.50  1920 200

8 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz e)

[3290118.103] (II) VIVANTE(0): Modeline "V:640x480p-60"x0.0   25.20  640 656 75

2 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.157] (II) VIVANTE(0): Output DISP3 BG has no monitor section

[3290118.158] (II) VIVANTE(0): Printing probed modes for output DISP3 BG

[3290118.158] (II) VIVANTE(0): Modeline "S:1920x1080p-60"x60.0  148.50  1920 20

08 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)

[3290118.158] (II) VIVANTE(0): Modeline "S:1920x1080p-50"x50.0  148.50  1920 24

48 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:1280x720p-50"x50.0   74.25  1280 172

0 1760 1980  720 725 730 750 +hsync +vsync -csync (37.5 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:1280x720p-60"x60.0   74.25  1280 139

0 1430 1650  720 725 730 750 +hsync +vsync -csync (45.0 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:720x576p-50"x50.0   27.00  720 732 7

96 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:720x480p-60"x59.9   27.00  720 736 7

98 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.157] (II) VIVANTE(0): Output DISP3 BG has no monitor section

[3290118.158] (II) VIVANTE(0): Printing probed modes for output DISP3 BG

[3290118.158] (II) VIVANTE(0): Modeline "S:1920x1080p-60"x60.0  148.50  1920 20

08 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)

[3290118.158] (II) VIVANTE(0): Modeline "S:1920x1080p-50"x50.0  148.50  1920 24

48 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:1280x720p-50"x50.0   74.25  1280 172

0 1760 1980  720 725 730 750 +hsync +vsync -csync (37.5 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:1280x720p-60"x60.0   74.25  1280 139

0 1430 1650  720 725 730 750 +hsync +vsync -csync (45.0 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:720x576p-50"x50.0   27.00  720 732 7

96 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:720x480p-60"x59.9   27.00  720 736 7

98 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "V:640x480p-60"x60.0   25.20  640 656 7

52 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.158] (II) VIVANTE(0): Modeline "S:640x480p-60"x59.9   25.17  640 656 7

52 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[3290118.158] (II) VIVANTE(0): Output DISP3 BG connected

[3290118.158] (II) VIVANTE(0): Using exact sizes for initial modes

[3290118.158] (II) VIVANTE(0): Output DISP3 BG using initial mode S:1920x1080p-

60

[3290118.158] (II) VIVANTE(0): imxDisplayPreInit: virtual set 1920 x 1080, disp

lay width 0

[3290118.158] (II) VIVANTE(0): FBDevPreInit: adjust display width 1920

[3290118.158] (**) VIVANTE(0): PreInit done

[3290118.158] (--) Depth 24 pixmap format is 32 bpp

[3290118.158] (II) VIVANTE(0): Init mode for fb device

[3290118.249] (II) VIVANTE(0): hardware: DISP3 BG (video memory: 16335kB)

[3290118.250] (II) VIVANTE(0): FB Start = 0x75610000  FB Base = 0x75610000  FB

Offset = (nil) FB PhyBase 0x76a00000

[3290118.250] (II) VIVANTE(0): reserve 8355840 bytes for on screen frame buffer

; total fb memory size 16727040 bytes; offset of shadow buffer 8355840

[3290118.325] (II) VIVANTE(0): hardware: DISP3 BG (video memory: 16335kB)

[3290118.340] (II) VIVANTE(0): test Initializing EXA

[3290118.340] (II) VIVANTE(0): (driver build from: -dirty)

[3290118.341] (II) EXA(0): Driver allocated offscreen pixmaps

[3290118.341] (II) EXA(0): Driver registered support for the following operatio

ns:

[3290118.341] (II)         Solid

[3290118.341] (II)         Copy

[3290118.341] (II)         Composite (RENDER acceleration)

[3290118.341] (II)         UploadToScreen

[3290118.341] (EE)

[3290118.341] (EE) Backtrace:

[3290118.341] (EE)

[3290118.341] (EE) Segmentation fault at address 0xd8

[3290118.341] (EE)

Fatal server error:

[3290118.341] (EE) Caught signal 11 (Segmentation fault). Server aborting

[3290118.341] (EE)

[3290118.341] (EE)

Please consult the The X.Org Foundation support

         at http://wiki.x.org

for help.

[3290118.341] (EE) Please also check the log file at "/var/log/Xorg.0.log" for

additional information.

[3290118.341] (EE)

[3290118.419] (EE) Server terminated with error (1). Closing log file.

0 Kudos