MMPF0100 LiCELL charge voltage and i.MX6 RTC operating voltage range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 LiCELL charge voltage and i.MX6 RTC operating voltage range

Jump to solution
1,347 Views
george
Senior Contributor II

Dear all,

When connecting rechargeable battery to MMPF0100 and using it as backup for RTC on i.MX6, the charge voltage to battery is 2.5V (default).

=> Page 113 on http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf

That is, battery voltage goes up to 2.5V.

When an external power supply is not connected to a system, RTC needs to work by Battery charged to 2.5V.

However, the operating voltage range of i.MX6 VDD_SNVS_IN is 2.9V-3.3V.

We keep only RTC.

Is really more than 2.9V needed in order to keep RTC?

I think that lower voltage is available in order to keep RTC operation generally.

If it becomes so, since it is necessary to change charge voltage setting to Battery more than 2.9V.

Best Regards,

George

Labels (1)
0 Kudos
1 Solution
682 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

yes it is necessary to change charge MMPF0100 voltage setting to

battery more than 2.9V since IMX6SDLCEC Table 9. Operating Ranges

defines backup battery supply range VDD_SNVS_IN as 2.9-3.3V

Also Table 8 Current Consumption Summary MMPF0100 datasheet :

Typical values are characterized at VIN = 3.6 V, VDDIO = 3.3 V, LICELL = 3.0 V,

VSNVS = 3.0 V and 25 °C, unless otherwise noted.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
683 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

yes it is necessary to change charge MMPF0100 voltage setting to

battery more than 2.9V since IMX6SDLCEC Table 9. Operating Ranges

defines backup battery supply range VDD_SNVS_IN as 2.9-3.3V

Also Table 8 Current Consumption Summary MMPF0100 datasheet :

Typical values are characterized at VIN = 3.6 V, VDDIO = 3.3 V, LICELL = 3.0 V,

VSNVS = 3.0 V and 25 °C, unless otherwise noted.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
682 Views
george
Senior Contributor II

Dear Igor,

Thanks.

BR

George

0 Kudos