IMX53 CPU :The Block Diagram shows there are 2 camaras Peripheral Interfaces ,but theres is only one csi peripheral,I want to conect 2 camaras ,how?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 CPU :The Block Diagram shows there are 2 camaras Peripheral Interfaces ,but theres is only one csi peripheral,I want to conect 2 camaras ,how?

1,005 Views
王凯王
Contributor I

IMX53 CPU  :The Block Diagram shows there are 2 camaras Peripheral Interfaces ,but theres is only one csi peripheral,I want to conect 2 camaras ,how?

0 Kudos
3 Replies

707 Views
igorpadykov
NXP Employee
NXP Employee

Hi 王凯 王

please look below

Re: Blurry image with CSI1 overlay

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

707 Views
王凯王
Contributor I

Thank you!

but there is only one csi (csidata0~csidata19 vsync hsync pix clk ) ,IF I conect two TVP5150 , how ?

I see "

Blurry image with CSI1 overlay

" they use two TVP5150

2014-10-20

wangkai

发件人: igorpadykov

发送时间: 2014-10-20 16:07:01

收件人: 王凯 王

抄送:

主题: Re: - IMX53 CPU :The Block Diagram shows there are2 camaras Peripheral Interfaces ,but theres is o

IMX53 CPU :The Block Diagram shows there are 2 camaras Peripheral Interfaces ,but theres is only one csi peripheral,I want to conect 2 camaras ,how?

reply from igorpadykov in i.MX Community - View the full discussion

Hi 王凯 王

please look below

Re: Blurry image with CSI1 overlay

Best regards

igor

0 Kudos

706 Views
igorpadykov
NXP Employee
NXP Employee

check i.MX53 Reference Manual (rev.2.1  6/2012)

sect.45.3 Features And Functionality

sect.45.3.1 External Ports :

IPU has the following ports:

• Two camera ports - each controlled by a CSI sub-block, providing a connection to

image sensors and related devices.

http://www.freescale.com/files/32bit/doc/ref_manual/iMX53RM.pdf

Table 4-3. Muxing Options sorted by IPs p.340 :  ports CSI0,CSI1

~igor

0 Kudos