i.MX6 Android (jb4.2.2._1.1.0) reboots automatically.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Android (jb4.2.2._1.1.0) reboots automatically.

Jump to solution
2,670 Views
satoshishimoda
Senior Contributor I

Hi community,

 

I have a question about i.MX6 Android BSP.
Actually, rarely android BSP reboots automatically if it is left without any operations.

 

[Board]
MCIMX6Q-SDP or MCIMX6DL-SDP

[BSP]
android_jb4.2.2_1.1.0-ga

[Procedure]
1. Boot Android BSP.
2. Tap "About tablet" in Settings menu 7 times, and "Developer options" become available.
3. Check "Stay awake".
4. Execute the following command from debug port to confirm android behavior.
# top -m 10 -d 5
5. Leave it without any operations.

[Result]
Android BSP rebooted without any error message as attached file.


[Question]
Do you know same issue?
Could you let me know how to avoid this issue?


Best Regards,
Satoshi Shimoda

Original Attachment has been moved to: [No.2]_20140324.log.zip

Labels (5)
1 Solution
1,585 Views
satoshishimoda
Senior Contributor I

Hi Yixing Kong,

> Had your issue got resolved?

Yes, this issue has resolved.

Actually, the root cause was GPT.

We modified GPT source code, and this issue was resolved.

Best Regards,

Satoshi Shimoda

View solution in original post

0 Kudos
13 Replies
1,585 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Can you remove the followed lines from init.rc to disable the watch dog? In this case, I think you can get the error logs.

# Set watchdog timer to 30 seconds and pet it every 10 seconds to get a 20 second margin

service watchdogd /sbin/watchdogd 10 20

    class core

1,585 Views
satoshishimoda
Senior Contributor I

Hi Qiang Li,

I got a report about this issue.

When watchdog is disabled, this issue was not occurred.

And we got a log that watchdog was NOT kicked about 7 min even though watchdog is set to be kicked every 10 sec.

Can you understand what is wrong these information?

Best Regards,

Satoshi Shimoda

0 Kudos
1,585 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The watchdogd is just a thread in Android, it just used sleep. The customer can find the source code:

system\core\init\watchdogd.c

    while(1) {

        write(fd, "", 1);

        sleep(interval);

    }

From my point, if there are many high priority tasks running with full CPU loading, there is chance that the watchdogs service has no time slot to run.

1,585 Views
satoshishimoda
Senior Contributor I

Hi Qiang Li,

Have you received a modified source code for test from Freescale local FAE?

Actually, a customer modify the watchdog source code and check the interval watchdog is kicked.

According to the test result with modified code, watchdog is kicked every 10 sec in normal , but 7 min interval was appeared.

We can understand higher priority tasks are executed before watchdog, but 7 min interval is too long.

So I guess some task prevents to kick the watchdog, or some task is stalled.

Then, could you let me know how to check what is prevents the watchdog kicking?

Best Regards,

Satoshi Shimoda

0 Kudos
1,585 Views
YixingKong
Senior Contributor IV

Satoshi-san

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
1,586 Views
satoshishimoda
Senior Contributor I

Hi Yixing Kong,

> Had your issue got resolved?

Yes, this issue has resolved.

Actually, the root cause was GPT.

We modified GPT source code, and this issue was resolved.

Best Regards,

Satoshi Shimoda

0 Kudos
1,585 Views
simon_cai
Contributor III

HI @Qiang_FSL

    does the GPT patch refer to this one 0025-ENGR00295714-GPT-Status-register-bits-are-cleared-in.patch.zip

thanks

0 Kudos
1,585 Views
chrissie
Contributor II

Hi satoshishimoda

     I have encountered the same issue as you commited, may I know how you sovle this issue? Did you modify the source code from fsl?

Or just modify some soure code you had modified before to freescale release source code?

     Thank you very much!

     Best Regards,

     Chrissie

0 Kudos
1,585 Views
satoshishimoda
Senior Contributor I

Hi Chrissie Jiang,

> Did you modify the source code from fsl?

Yes, I got a patch to modify GPT source code from local Freescale FAE.

So I recommend you contact to a local Freescale FAE and get the GPT patch.

Best Regards,

Satoshi Shimoda

0 Kudos
1,585 Views
chrissie
Contributor II

Hi Satoshi Shimoda,


     I will contact local Freescale FAE immediately.Thank you very much!

     Best Regards,

     Chrissie

0 Kudos
1,585 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

After removed the wdog services from init.rc, no one will kick watchdog, so it is reasonable.

0 Kudos
1,585 Views
LeonardoSandova
Specialist I

Any error log shown by watchdog?

0 Kudos
1,585 Views
satoshishimoda
Senior Contributor I

Hi Leonardo,

I'm checking whether watchdog outputs some error or not.

Just a moment, please?

Best Regards,

Satoshi Shimoda

0 Kudos