Hi, I cannot use OPENOCD Debug with FRDM-K64 in kds 1.1.0, the program cannot download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, I cannot use OPENOCD Debug with FRDM-K64 in kds 1.1.0, the program cannot download

1,672 Views
kehanqin-b46569
NXP Employee
NXP Employee

HI, KDS experts

I download the KDS 1.1.0 version last week, create a simple project of FRDM-K64 try to debug via OPENOCD, CMSIS-DAP, strangely it's failed but back to KDS 1.0.1 there is no such issue.

The program cannot download in chip but in KDS the state is RUN without stop before main, meantime, the green-led of SDA on board is blinking. but program still hasn't downloaded.

14054_14054.png1.png

 

below is my setting and failed infos

 

Open On-Chip Debugger 0.8.0-dev-00003-g0c51359 (2014-07-25-13:18)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'cmsis-dap'

Info : CMSIS-DAP: SWD  Supported

Info : CMSIS-DAP: Interface Initialised (SWD)

Info : add flash_bank kinetis k64.flash

cortex_m reset_config sysresetreq

adapter speed: 50 kHz

Warning - This configuration file is deprecated and will be removed in future versions, use kinetis.cfg instead.

Info : CMSIS-DAP: FW Version = 1.0

Info : SWCLK/TCK = 0 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1

Info : DAP_SWJ Sequence (reset: 50+ '1' followed by 0)

Info : CMSIS-DAP: Interface ready

Info : clock speed 50 kHz

Info : IDCODE 0x2ba01477

Info : k64.cpu: hardware has 6 breakpoints, 4 watchpoints

Info : accepting 'gdb' connection from 3333

target state: halted

target halted due to debug-request, current mode: Handler HardFault

xPSR: 0x61000003 pc: 0x00000568 msp: 0x1fffc3d0

Info : Probing flash info for bank 0

Warn : acknowledgment received, but no packet pending

target state: halted

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x00000530 msp: 0x1fffc400

semihosting is enabled

Warn : Any changes to flash configuration field will not take effect until next reset

target state: halted

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x00000530 msp: 0x20000920, semihosting

 

and this is my debug configuration of OPENOCD

About config options, I use "-f kinetis.cfg" before, but make no sense,too.

14055_14055.png2.png

 

But KDS 1.0.1 was fine.

 

Please help, thanks a lots!

Labels (1)
Tags (3)
0 Kudos
2 Replies

476 Views
BlackNight
NXP Employee
NXP Employee

Further comment on your debug screenshot: what does it show if you press the 'pause' button.

I suspect you might not have allocated enough HEAP space in the linker file, and that the program is stuck in the startup code?

Erich

0 Kudos

476 Views
BlackNight
NXP Employee
NXP Employee

Hello,

with KDS V1.1.0, you really should use

-f kinetis.cfg

I have posted an example in this thread using printf:

First impression with KDS 1.1.0 Can't Debug FRDM-K64F with OpenOCD/CMSIS-DAP

which has all the debug configurations (Segger/J-Link/OpenOCD) configured.

Can you try it?

Additionally, try to power-unpower-power the FRDM-K64F board.

I hope this helps,

Erich

0 Kudos