Hi
I've used the BSP Cloning wizard to generate a cloned version of the TWRK60D100M board.
I then copied the .xml file (from CodeWarriorNPW) into the codewarrior folder structure at
<codewarrior_install_dir>/MCU/lib/wizard_data/mqx/4.1/arm
but when I run the new project wizard in codewarrior, the new board doesn't appear in the select board list.
I'm running Codewarrior 10.6 on Windows 7
I've tried to examine the Windows registry at
[HKEY_LOCAL_MACHINE\SOFTWARE\Freescale\Freescale MQX]
but there is no Freescale directory listed.
Can someone please...?
Thanks
Hi Ken,
Are you using 32-bit Windows or 64-bit Windows? If you are using 32-bit Windows then you can follow the document that Daniel shared, however if you are using 64-bit windows then you need to check the below thread:
Custom BSP with MQX 4.0.1 and CW 10.4
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ken,
I had issues with Windows7 64-bit machines allowing the *.reg file to be used and the result of my findings is that the BSPCloningWizard is only generating Windows7 32-bit *.reg files. Below is how I edited the *.reg file to be used with Windows7 64-bit machine.
My assumption is this process works with CW10.6 as well.
Hope this helps.
The BSPCloningWizard is being updated in the MQX4.1 release to provide a 32-bit and 64-bit registry file.
You can make the edit to your *.reg file to have it load correctly for 64-bit machine. I’ve attached my original *.reg and modified *_64.reg files for reference.
I tested it as follows:
The steps I used to have the custom board show up for use in new MQX4.0 projects are:
From the BSP port on my machine (Windows7 64-bit) I did for you I did the following specific steps:
To view the Windows 64-bit registry I’ve attached PDF from Microsoft that explains how to open correct “regedit”.
Regards,
David
Thanks Dave - sorted...
Hi
Please check the attached document for adding cloned BSP to CodeWarrior Project
Have a great day,
Daniel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------