i.MX6DQ QuadSPI boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ QuadSPI boot.

Jump to solution
763 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ.

Please see chapter 8.6 in IMX6DQRM Rev.2, it say i.MX6DQ can QuadSPI boot.

However, there is no description about QuadSPI other than this chapter.

And according to Quad SPI availability with iMX6, i.MX6 cannot use QuadSPI.

Is chapter 8.6 misprint? or i.MX6DQ was updated to use QuadSPI?

If i.MX6DQ can use QuadSPI boot, could you let me know the connection and IOMUX setting also?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
552 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

sorry i.MX6DQ can not use QuadSPI boot,

IMX6DQRM Rev.2 has misprint (this material is from next IMX6SLXRM).

Best regards

chip
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
553 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

sorry i.MX6DQ can not use QuadSPI boot,

IMX6DQRM Rev.2 has misprint (this material is from next IMX6SLXRM).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos