First, it complained about an old org.eclipse.core.runtime dependency.
I installed org.eclipse.core.runtime, and fixed that issue, and it still fails to install the plugin.
Cannot complete the install because one or more required items could not be found.
Software currently installed: Freescale MQX support for ARM DS-5 1.0.2.201307020935 (com.freescale.mqx.ds5.feature.group 1.0.2.201307020935)
Missing requirement: MQX Configuration Editor 1.1.6.201307020935 (com.freescale.mqx.configuration.editor 1.1.6.201307020935) requires 'bundle org.eclipse.core.runtime [3.7.0,3.8.0)' but it could not be found
Cannot satisfy dependency:
From: Freescale MQX support for ARM DS-5 1.0.2.201307020935 (com.freescale.mqx.ds5.feature.group 1.0.2.201307020935)
To: com.freescale.mqx.configuration.editor [1.1.6.201307020935]
i cannot find any (com.freescale.mqx.configuration.editor) install site or download
using 4.1 w/ patch 4.1.0.1
DS-5 5.19.0
Vybrid tower.
Solved! Go to Solution.
This line:
Missing requirement: MQX Configuration Editor 1.1.6.201307020935 (com.freescale.mqx.configuration.editor 1.1.6.201307020935) requires 'bundle org.eclipse.core.runtime [3.7.0,3.8.0)' but it could not be found
means that MQX Configuration Editor is dependent on Eclipse v3.7 to 3.8.
DS-5 v5.18 and v5.19 uses Eclipse v4.3, so you have two options:
- Use DS-5 v5.17, which had Eclipse v3.7. You can find it in the "Older Releases" tab here: http://ds.arm.com/downloads/
- Contact Freescale for information on whether they're planning to update MQX Configuration Editor to support Eclipse 4.3.
or use this
Hi David,
Please check the attached document and let me know if this helps.
In addition, according with the release notes Freescale MQX RTOS was compiled and tested with
DS-5 Starter Kit for Vybrid Controllers version 5.16.0
DS-5 Vybrid Controller Edition 5.16.0
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
This line:
Missing requirement: MQX Configuration Editor 1.1.6.201307020935 (com.freescale.mqx.configuration.editor 1.1.6.201307020935) requires 'bundle org.eclipse.core.runtime [3.7.0,3.8.0)' but it could not be found
means that MQX Configuration Editor is dependent on Eclipse v3.7 to 3.8.
DS-5 v5.18 and v5.19 uses Eclipse v4.3, so you have two options:
- Use DS-5 v5.17, which had Eclipse v3.7. You can find it in the "Older Releases" tab here: http://ds.arm.com/downloads/
- Contact Freescale for information on whether they're planning to update MQX Configuration Editor to support Eclipse 4.3.
or use this