i.MX6 PCIe can't detect issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 PCIe can't detect issue.

Jump to solution
1,654 Views
edwinrose
Contributor I

Hi experts,

I meet a question about PCIE bus on i.MX6.

1. When I inserted Intel EXPI9301CTBLK PCI-Express(x1) Network Adapter in my board, it can works.

2. Insert Realtek RTL8111E PCIE LAN card, the system can't detect this device, following is the console message.

2014-7-2 下午 05-19-36.jpg

Could you help us to see what is the problem for this issue?

BSP version: imx_3.0.35_4.1.0

Thanks for your help.

Labels (2)
Tags (1)
0 Kudos
1 Solution
765 Views
igorpadykov
NXP Employee
NXP Employee

Hi edwin

please try solutions given in link below

mx6 + rtl8111e driver

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
766 Views
igorpadykov
NXP Employee
NXP Employee

Hi edwin

please try solutions given in link below

mx6 + rtl8111e driver

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
765 Views
edwinrose
Contributor I

I have solved this issue, thanks for your help.

0 Kudos