What Voltage should NVCC_1P2V be on the SoloLite?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What Voltage should NVCC_1P2V be on the SoloLite?

Jump to solution
952 Views
bjozwiak
Contributor I

Sounds like the answer is in the question. But the new version of the SoloLite Datasheet (REV3) has confused the situation. On page 21 of the Rev3 datasheet it seems to be tied to the DDR interface voltage. Should this pin (W7; NVCC_1P2V) be tied to the voltage we use for DDR? Or should it be 1.2V?

Also what is the 1.2V power pin used for in the SoloLite? The datasheet is unclear. It looks like it is used for the HSIC interface. It also looks like it can be used for the internal 24MHz Oscillator. DDR?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
806 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bryan

yes,  pin (W7; NVCC_1P2V) may be tied to the voltage you use for DDR

or use the same voltage value from other power source.

I did not fully understand question:

"what is the 1.2V power pin used for in the SoloLite".

Table 73 "13 x 13 mm Functional Contact Assignments"

SoloLite Datasheet (REV3) gives power domains for all pads.

Yes, NVCC_1P2V is used for the HSIC interface, others - not.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
807 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bryan

yes,  pin (W7; NVCC_1P2V) may be tied to the voltage you use for DDR

or use the same voltage value from other power source.

I did not fully understand question:

"what is the 1.2V power pin used for in the SoloLite".

Table 73 "13 x 13 mm Functional Contact Assignments"

SoloLite Datasheet (REV3) gives power domains for all pads.

Yes, NVCC_1P2V is used for the HSIC interface, others - not.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply