Hello
I have written about my problems with embedded subtitles https://community.freescale.com/thread/317604 . However I also have problem with playing external subtitles. The file containing the video is an mkv file. I can play its video with no problem. The subtitles are in a .srt file. I can play it on my linux box with
gst-launch-0.10 filesrc location = /mnt/hgfs/work/test_videos/Tales.from.Earthsea\[h264.dts\]\[niizk\].mkv ! decodebin2 name=dec ! subtitleoverlay name=overlay ! ffmpegcolorspace ! autovideosink filesrc location = /mnt/hgfs/work/test_videos/Tales.from.Earthsea.srt name=subfile ! subparse ! overlay.
However when I try to play the file on my i.MX6 board with
gst-launch-0.10 filesrc location = /mnt/sdb1/kur/Tales.from.Earthsea\[h264.dts\]\[niizk\].mkv ! decodebin2 name=dec ! subtitleoverlay name=overlay ! ffmpegcolorspace ! mfw_v4lsink filesrc location = /mnt/sdb1/kur/Tales.from.
Earthsea.srt name=subfile ! subparse ! overlay.
It exits immediately with the following printed:
MFW_GST_V4LSINK_PLUGIN 3.0.5 build on Oct 22 2013 15:33:00.
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
ERROR: from element /GstPipeline:pipeline0/GstFileSrc:subfile: Internal data flow error.
Additional debug info:
gstbasesrc.c(2582): gst_base_src_loop (): /GstPipeline:pipeline0/GstFileSrc:subfile:
streaming task paused, reason not-negotiated (-4)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Total rendered:0
Aiur: 3.0.5
Core: MKVPARSER_01.04.01 build on Dec 10 2012 15:43:34
mime: video/x-matroska ; video/webm
file: /usr/lib/imx-mm/parser/lib_mkv_parser_arm11_elinux.so
Content Info:
URI:
file:///mnt/sdb1/kur/Tales.from.Earthsea[h264.dts][niizk].mkv
Idx File:
/root/.aiur/.mnt.sdb1.kur.Tales.from.Earthsea[h264.dts][niizk].mkv.aidx
Seekable : Yes
Size(byte): 2100598489
[--->FINALIZE aiurdemux
Freeing pipeline ...
[--->FINALIZE v4l_sink
I have no Idea what that means. Can somebody help with this?
I attach the subtitles file in case it is needed for identifying the problem.
Lachezar
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Lachezar
We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Lachezar
Is this post the same issue with https://community.freescale.com/thread/3176074? If yes, we are going to close this one and leave that one open for someone to answer.
Thanks,
Yixing