VF65GS10 power design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF65GS10 power design

Jump to solution
761 Views
RsBogdan
Contributor I

SR Number: 1-1093845751
Date Opened: 17-Jul-2013 03:57:42 PM
Subject: VF65GS10 power design
Description: Customer is currenlty desiging with VF65GS10 and was aware that theVF65GS10 tower board was delayed to production. Rumor is that there was an issue in the power solution for this board .. the customer would like to know any details so that they dont have the same issue.

Labels (1)
0 Kudos
1 Solution
623 Views
naoumgitnik
Senior Contributor V

Dear RsBogdan,

Below is an excerpt from the older 'Re: About the issue of TWR-VF65GS10 power supply circuit' thread:

  1. If your customer does not use USB as a power source, all the below information is irrelevant.
  2. The issue was with a type of the previously used Switch IC controlling the USB power on the board - MIC2026, whose built-in current threshold appeared to be marginal for the latest SW applications, so it had to be replaced with a drop-in replacement, MIC2506, with a higher threshold.
  3. The next schematic revision (in progress) with MIC2506 instead of MIC2026 will be G1.

Best regards, Naoum Gitnik.

View solution in original post

0 Kudos
1 Reply
624 Views
naoumgitnik
Senior Contributor V

Dear RsBogdan,

Below is an excerpt from the older 'Re: About the issue of TWR-VF65GS10 power supply circuit' thread:

  1. If your customer does not use USB as a power source, all the below information is irrelevant.
  2. The issue was with a type of the previously used Switch IC controlling the USB power on the board - MIC2026, whose built-in current threshold appeared to be marginal for the latest SW applications, so it had to be replaced with a drop-in replacement, MIC2506, with a higher threshold.
  3. The next schematic revision (in progress) with MIC2506 instead of MIC2026 will be G1.

Best regards, Naoum Gitnik.

0 Kudos