Vybrid Boot pin setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid Boot pin setting

Jump to solution
1,112 Views
AhmedShameemM_H
Contributor I

Dear Sir,


In Freescale Tower system module, there is buffer used for isolation (see attachment) on Vybrid Boot setting pins.But for other Freescale processor’s reference boards like i.MX53 QSB, i.MX6 SDB etc. usually resistor isolation only provided.Buffer is must or Is there any specific reason for using this buffer in Vybrid reference board?

Waiting for your valuable feedback.

Thank You, in advance.

Regards,

Shameem

Labels (2)
0 Kudos
1 Solution
807 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Shameem,

  See this thread for an explanation for the buffers: Re: Vybrid GPIO Boot override

-Anthony

View solution in original post

0 Kudos
2 Replies
808 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Shameem,

  See this thread for an explanation for the buffers: Re: Vybrid GPIO Boot override

-Anthony

0 Kudos
807 Views
AhmedShameemM_H
Contributor I

Thank you , Anthony

0 Kudos