nand_flash mqx demo doesn't work on K70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nand_flash mqx demo doesn't work on K70

Jump to solution
1,016 Views
lorenzofornari
Contributor III

Hello, i've tried the nand_flash demo, provided in "example" folder in mqx 4.0.

The demo works properly only if you don't generate processor expert code.

Whether PE code is generated, the application finds bad all blocks, and cannot write or read correclty from them.

Simply deleting generated code and rebuilding bsp, makes the demo working properly again.

I've deleted all components in PE configuration, leaving only mqx and cpu,with the same result.

I think there are some conflicts, but i haven't yet found where...

Some ideas?

Thanks

1 Solution
607 Views
Martin_
NXP Employee
NXP Employee
0 Kudos
3 Replies
608 Views
Martin_
NXP Employee
NXP Employee

It is caused by the NFC clock divider. Solution:

https://community.freescale.com/message/335347#335347

0 Kudos
607 Views
lorenzofornari
Contributor III

ok, thanks Martin, now it works.

0 Kudos
607 Views
friederschrempf
Contributor IV

I had the same problems. See here: Re: FFS on NANDFLASH of TWR-K70 (MQX 4.0.1)