Goodmorning everybody,
I've downloaded LTIB version L2.6.35_11.03_ER_source_bundle.tar.gz and I've tried to install it by the basic commands:
./ltim -m config
./ltib
When I set QT installation (with or without X11 support), ltib can't find link for sources:
#./ltib
...
Try qt-everywhere-opensource-src-4.6.0.tar.gz.md5 from the GPP
http://bitshrine.org/gpp/qt-everywhere-opensource-src-4.6.0.tar.gz.md5:
23:55:55 ERROR 404: Not Found.
Try qt-everywhere-opensource-src-4.6.0.tar.gz from the GPP
http://bitshrine.org/gpp/qt-everywhere-opensource-src-4.6.0.tar.gz:
23:55:56 ERROR 404: Not Found.
Can't get: qt-everywhere-opensource-src-4.6.0.tar.gz at ./ltib line 790.
So, URL is broken.
I've tried to download qt-everywhere-opensource-src-4.6.0.tar.gz from web and copy it in /opt/freescale/pkgs. But its compilation fails:
#./ltib
...
The specified system/compiler is not supported:
/home/user/Documents/L2.6.35_11.03_ER_source_bundle/ltib/rpm/BUILD/qt-everywhere-opensource-src-4.6.0/mkspecs/qws/linux-g++-mx
Please see the README file for a complete list.
error: Bad exit status from /home/user/Documents/L2.6.35_11.03_ER_source_bundle/ltib/tmp/rpm-tmp.96334 (%build)
RPM build errors:
Bad exit status from /home/user/Documents/L2.6.35_11.03_ER_source_bundle/ltib/tmp/rpm-tmp.96334 (%build)
Build time for qt-embedded: 0 seconds
Failed building qt-embedded
So, where is a valid repository url for qt-everywhere-opensource-src-4.6.0.tar.gz ?
please check this link https://community.freescale.com/thread/300825 to see if it's helpful.
Your linked page shows how to install Qt manually instead of using "ltib - m config".
But the page is not clear: where is the link to download "mkspec package"?
The following may be helpful :