I have Installed a device ram , under which I have installed a MFS named "s:"
Then I am uninstalling "s:".
I want to search all the files present in he device . so, I am opening ram using fopen & searching first file using ioctl , which is throwing error .
I am writing a code to search a file from root directory.
mfs_ramdisk: is device driver , the directory is a:(only root directory is present no other directory is present)
error_code = ioctl(mfs_fd_ptr, IO_IOCTL_FIND_FIRST_FILE,(uint_32_ptr) &search);// I am getting error in this statement , it is failing and not displying any files searched
mfs_fd_ptr = fopen("ramdisk:", NULL); |
if (mfs_fd_ptr == NULL)
{
printf("Error opening the MFS device driver!"); | |
return; |
}
error_code = ioctl(mfs_fd_ptr, IO_IOCTL_FIND_FIRST_FILE,(uint_32_ptr) &search);
while (error_code == MFS_NO_ERROR)
{
error_code = ioctl(mfs_fd_ptr, IO_IOCTL_FIND_NEXT_FILE,(uint_32_ptr) &search_data); |
}
fclose(mfs_fd_ptr);
Thanks in advance
Solved! Go to Solution.
Hi netra,
Why are you closing "s:"?
Have you reviewed and run the following example?
C:\Freescale\Freescale_MQX_4_0\mfs\examples\ramdisk\cw10
From the shell prompt, after you have formatted the drive, you can create a test file and the issue a "dir" shell command that will issue the IOCTL command to find the first file in current directory.
Here is my terminal output (note I used TWR-MEM card with MRAM):
shell> Demo start
Initialized Ram Disk to a:\
NOT A DOS DISK! You must format to continue.
Shell (build: Feb 15 2013)
Copyright (c) 2008 Freescale Semiconductor;
shell>
shell> format a:
Formating...
Done. Volume name is
Free disk space: 518144 bytes
shell>
shell> dir
shell>
shell> write test.txt 123
shell>
shell> dir
TEST.TXT 123 01-01-1980 00:04:26 A TEST.TXT
shell>
Similar topic that might also be of value:
Re: USB device with MFS ramdisk
Hope this helps.
Regards,
David
Netra, is this helpful?
How is the project going?
Keep us posted please! :smileywink:
Regards!
Hi netra,
Why are you closing "s:"?
Have you reviewed and run the following example?
C:\Freescale\Freescale_MQX_4_0\mfs\examples\ramdisk\cw10
From the shell prompt, after you have formatted the drive, you can create a test file and the issue a "dir" shell command that will issue the IOCTL command to find the first file in current directory.
Here is my terminal output (note I used TWR-MEM card with MRAM):
shell> Demo start
Initialized Ram Disk to a:\
NOT A DOS DISK! You must format to continue.
Shell (build: Feb 15 2013)
Copyright (c) 2008 Freescale Semiconductor;
shell>
shell> format a:
Formating...
Done. Volume name is
Free disk space: 518144 bytes
shell>
shell> dir
shell>
shell> write test.txt 123
shell>
shell> dir
TEST.TXT 123 01-01-1980 00:04:26 A TEST.TXT
shell>
Similar topic that might also be of value:
Re: USB device with MFS ramdisk
Hope this helps.
Regards,
David