hai for the last few days i was trying to install the ltib package for i.mx28...but the installation failed and the following errors were shown:
------- | ----------- --------------- | |
glibc-devel | 0 | not installed |
zlib | 0 | not installed |
Died at ./ltib line 1397.
traceback:
main::host_checks:1397
main:542
Started: Thu Feb 7 15:39:38 2013
Ended: Thu Feb 7 15:39:38 2013
Elapsed: 0 seconds
Build Failed
i am using ubuntu12.04 and i dont know how to resolve this issue........from the posts i have seen i doubt if i will be able to install the ltib package in ubuntu 12.04.....should i switch on to ubuntu 10.04 or 10.10.....i used the following linux bsp guide to install the ltib packages.....
please do help i am in need.......
thanks
catherine g f
Hi Catherine,
I remember there are patches on the community regarding this issue. Please take a look at this file
bin/Ltibutils.pm
Search for those two strings: zlib and glibc-devel ADD the correct path in each case. The correct path can be found using the command 'find' from a shell on your Ubuntu Host.
Let us know if you have success.
Leo
The following (about i.MX53 QSB) may help - it works for i.MX28 LTIB too.
Ubuntu 11.10 Oneiric 64-bit Virtual Machine and building i.MX53 L2.6.35-11-09-01
Hello Catherine,
I have also done successful installation of LTIB in Ubuntu 10.04.We need certain packages to be installed in Ubuntu which are required for installation of LTIB else it would fail.
Also after installation of packages there if a fix given for installing LTIB in 12.04 on i.MX Community itself.Please follow that also.
Thanks,
Saurabh