I am compiling a project for the MCF52255AF80 with the MQX RTOS. I have compiled the m52259demo_libs to recompile the MQX kernal; however, when I compile my project I get support_common.h cannot be opened. I looked through the included files and it is missing. Where can I find this file to include it?
Thanks for your help.
Type "support_common.h" into the Search Box in this forum and see if Jim's instructions help you in this match:
Re: MC52235 Serial Port Communications
Check some of the other matches in case they help.
Which files are trying to include the missing one?
Tom
Thanks for the help.
I was able to get that to work. However; once I build the project in debug it works then once I build it in release it says it cannot open enetprv.h.
Thanks,
Blake
The file that is trying to include this is Bootloader_V2.h. In fact the
bootloader files are were my errors are coming from.