I want to decode WMA/WMV file to try to check for windows media files.
Where can I find the WMV/WMA codec support ?
I can't find out these in the LTIB package when building with MMCODEC.
If it needs license agreement, do we have to contact microsoft ?
Best Regards,
kanou
Solved! Go to Solution.
Please apply to local Freescale FAE.
Windows Media Components Final Product Licensee should be approved prior to distribution.
Please apply to local Freescale FAE.
Windows Media Components Final Product Licensee should be approved prior to distribution.
Dear I.MX Community,
I am using L2.6.35_1.1.0_130130_source for my I.MX28 customized platform,
I am trying to play .wma songs using gplay, but the .wma songs which has album art is not playing, & .wma songs which has metadata is also not getting played,
As am new to this .wma software codec, could you please let me know how to resolve this issue, & necessary configurations that is to be done
in the ltib, inorder to get the the wma songs with album art & metadata getting played
Could you please let me know the detailed ltib configurations that needs to be done in order to get the wma songs to be played with album art & metadata
WMA with album art not working LOGs
gplay test.wma
playbin2 is employed!
fsl_player_init(): Successfully initialize!
fsl_player_set_media_location(): filename=/03 - Mahiya - Suzzane.wma
[Stopped ][Vol=01][00:00:00/00:00:00][fps:0]Aiur: 3.0.6
Core: ASFPARSER_01.00.14 build on Dec 10 2012 15:58:36
mime: video/x-ms-asf
file: /usr/lib/imx-mm/parser/lib_asf_parser_arm9_elinux.so.3.1
Content Info:
URI:
file:///03 - Mahiya - Suzzane.wma
Idx File:
/root/.aiur/.03 - Mahiya - Suzzane.wma.aidx
Seekable : Yes
Size(byte): 1657511
[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4
[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4
[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4
[Stopped (List Repeated)][Vol=01][00:00:00/00:00:00][fps:25]Wait status change from 2 to 4
Please kindly do the needful as early as possible, as am stuck with this from many days,
Many Advanced Thanks,