How do i see USB_OTG enabled device files in linux-imx?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do i see USB_OTG enabled device files in linux-imx?

858 Views
anush_deekonda
Contributor I

Hi,

I am using yocto sumo version linux kernel.

I enabled the following OTG configuation in menuconfig:

/********************************************************

Symbol: USB_OTG [=y] x
x Type : boolean x
x Prompt: OTG support x
x Location: x
x -> Device Drivers x
x -> USB support (USB_SUPPORT [=y]) x
x (8) -> Support for Host-side USB (USB [=y]) x
x Defined at drivers/usb/core/Kconfig:44

**********************************************************/

1. What is the device file i can expect in the rootfs with the above change?

2. What are the usb device files needed for communicating with MFG/UUU tool and how do i enable that in the kernel(I see /dev/utp missing)?

Thank you,

Anush D.

#fsl_utp

#usb_otg

#mfgtools

#yocto sumo

Labels (3)
0 Kudos
1 Reply

778 Views
jimmychan
NXP TechSupport
NXP TechSupport

If you want to build the firmware for mfgtool, please refer to this thread.

https://community.nxp.com/message/1042399 

0 Kudos