iMX8M mini + 2GB DDR4 boot problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M mini + 2GB DDR4 boot problems

848 Views
giacomobiancala
Contributor I

Dear all,

I have some booting problems on my custom board based on iMX8M mini processor.

We use PMIC PCA9450.

Processor code MIMX8MM5DVTLZAA

DDR4 DRAM code (2GB total): 2 x MT40A512M16LY-075:E

DRAM Schematics connections is the same than EVK SCH-35104_B1  (8MMINID4-CPU).

We set main voltage as follows:

- VDD_DRAM&PU = 0,9V

- VDD_DRAM_1V2 = 1,2V

We produced 14 prototipes of this board. 10 boards always boot properly and they have no problems.

The other 4 boards do not boot properly every time. Console output is following:

U-Boot SPL 2018.03-g5f7f913-dirty (Jul 03 2020 - 13:57:13 +0200)
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
DRAM PHY training for 2400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED

There are 2 FAILED on DRAM test so the boot process stops.

If I run RAM Stress Test "mscale_ddr_tool_v310_setup.exe" (both calibration and Stress Test) all works fine so it seems that DDR4 connections have no problems but when I use the UBOOT the booting stops after RAM tests in SPL (only on this 4 boards).

Could you help me?

Thanks

Giacomo

Labels (1)
0 Kudos
1 Reply

693 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo

if only some boards do not boot properly, this may be poor soldering issue,

one can try to test boards with x-ray screening.

Alternatively one can try to tweak drive strength and ODT parameters using

RPA tool on i.MX 8M Family DDR Tool Release 
Check power supply noise or spikes – refering to HW Developers Guide

i.MX 8M Mini Hardware Developer’s Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos