Violet screen when using iMX6S + TP2854 + Camera HDTVI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Violet screen when using iMX6S + TP2854 + Camera HDTVI

966 Views
toanjunifer
Senior Contributor I

Hi,

I'm trying to use Camera HDTVI with TP2854 in iMX6S(Linux 4.1.15). After try some example program in unit_test folder, such as: 

   $ ./mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 & sleep 10

I get only violet screen:

violet.jpeg

Someone can tell me why does it happened ? And how to fix it ?

Thank you so much,

Toan

Labels (1)
3 Replies

856 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dao

one can look at below link:

iMX6DQ TP2854 MIPI CSI2 720P HD-TVI camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

856 Views
toanjunifer
Senior Contributor I

Thank you igorpadykov‌, I read this article before but it does solve my problem. Do you have any suggestions ? 

Thanks in advance,

Toan

0 Kudos

856 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dao

 

one can debug it running in parallel this demo and custom board and

comparing ipu registers, use as additional help

Using Open Source Debugging Tools for Linux on i.MX Processors

 

Best regards
igor