Hi,
I could could not get the DDR Test Tool to connect to the USB Device. It is set to serial boot, and I can down uboot and linux using uuu. However, DDR Test Tool kept giving me ERROR: Can't Open USB device. The following are the setting
* Connected to USB OTG
* Configure to Serial booting (I even verified that uuu can detect usb otg)
* Loaded init script EVK_IMX6ULL_DDR3L_400MHz_512MB_16bit_V1.2.inc
* Select TARGET: MX6ULL
I wonder if I missed any steps
Hi Tan
one can try on different PC, also please try first power-up
board then attach usb cable to computer. May be useful below presentation
showing usage ddr test step by step
https://community.nxp.com/docs/DOC-331528
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for quick reply.
Actually, I found a problem on one of my machines. I did try on a desktop PC and a laptop, both didn't not work. However, I found the virtualbox that I use for debugging uboot using the USB-OTG debugging for IMX, seems rename the usb drive in windows to virtualUSB, and DDR Test Tool does not seems to like it. When VirtualBox was closed, DDR Test Tool was able to detect USB.
However, I still don't know what was wrong on my PC, but probably something similar or driver related.
Tan